Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Starting a application with u-boot on Microzed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 365 subscribers
  • Views 1656 views
  • Users 0 members are here
Related

Starting a application with u-boot on Microzed

e14 Contributor
e14 Contributor over 10 years ago

Hi,
I'm trying to start a RTEMS application on the Microzed Board with u-boot. The .bin file is located on the SD card. I try it the following way:
  1. fatload mmc 0 0x100000 ticker.bin
  2. go 100000
Than it freezes with:
## Starting application at 0x00100000 ...

When I try to bootm the image of ticker.bin with:
  1. fatload mmc 0 100000 ticker.img
  2. bootm 100000
it freezes with:
## Booting kernel from Legacy Image at 00100000 ...                                          
   Image Name:   RTEMS Application                                                           
   Image Type:   ARM RTEMS Kernel Image (uncompressed)                                       
   Data Size:    1039080 Bytes = 1014.7 KiB                                                  
   Load Address: 30000100                                                                    
   Entry Point:  30000100                                                                    
   Verifying Checksum ... OK                                                                 
   Loading Kernel Image ... OK                                                               
OK                                                                                           
## Transferring control to RTEMS (at address 30000100) ...

I use the U-Boot 2013.01-dirty version of u-boot. RTEMS is a bare metal application

Regards

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Arturete,

    Is your SD card the one that came packaged with the Zedboard? If not is it formatted to FAT32?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • arturete
    0 arturete over 9 years ago in reply to jafoste4

    I'm not sure if this the SD is the original from the kit because I'm working in the university and we are some people working with different SDs.

    But yes It is formatted with FAT32

    If I print the partition table of the SD with fdisk this is the result:

    arturete@ubuntu:~$ sudo fdisk /dev/sdc

    Command (m for help): p

    Disk /dev/sdc: 3991 MB, 3991928832 bytes
    83 heads, 45 sectors/track, 2087 cylinders, total 7796736 sectors
    Units = sectors of 1 * 512 = 512 bytes
    Sector size (logical/physical): 512 bytes / 512 bytes
    I/O size (minimum/optimal): 512 bytes / 512 bytes
    Disk identifier: 0x1bb12714

       Device Boot      Start         End      Blocks   Id  System
    /dev/sdc1   *        2048     7796735     3897344    b  W95 FAT32
     

    And I'm sure that I am connected to the board through gkterm because the UART led (RX) blink when I press enter. But the other led never blink(TX) when or after the board is booted.

    Thanks for the fast reply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • arturete
    0 arturete over 9 years ago in reply to jafoste4

    I'm not sure if this the SD is the original from the kit because I'm working in the university and we are some people working with different SDs.

    But yes It is formatted with FAT32

    If I print the partition table of the SD with fdisk this is the result:

    arturete@ubuntu:~$ sudo fdisk /dev/sdc

    Command (m for help): p

    Disk /dev/sdc: 3991 MB, 3991928832 bytes
    83 heads, 45 sectors/track, 2087 cylinders, total 7796736 sectors
    Units = sectors of 1 * 512 = 512 bytes
    Sector size (logical/physical): 512 bytes / 512 bytes
    I/O size (minimum/optimal): 512 bytes / 512 bytes
    Disk identifier: 0x1bb12714

       Device Boot      Start         End      Blocks   Id  System
    /dev/sdc1   *        2048     7796735     3897344    b  W95 FAT32
     

    And I'm sure that I am connected to the board through gkterm because the UART led (RX) blink when I press enter. But the other led never blink(TX) when or after the board is booted.

    Thanks for the fast reply.