Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development U-boot QSPI read speed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 701 views
  • Users 0 members are here
Related

U-boot QSPI read speed

e14 Contributor
e14 Contributor over 12 years ago

I have built an design for the Zedboard that boots Linux from the QSPI flash. The loading time for my 8 MB ramdisk image is 26 seconds which would give a bandwidth of about 300kB/s which seems to be very slow. The SD card boots in a couple of seconds and according to what I've read the QSPI should be faster. Any thoughts of what speed to expect or any ideas of where to tweak to increase the speed of the QSPI flash read operation?

Thanks!
/Roger

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I can add that the version of the U-boot is 2014.01 and I am using vivado 2014.2. When i do the same read operation in Linux after boot using cp /dev/mtdX the read time is a third of the u-boot read time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I can add that the version of the U-boot is 2014.01 and I am using vivado 2014.2. When i do the same read operation in Linux after boot using cp /dev/mtdX the read time is a third of the u-boot read time.