Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development when using AXI DMA,the devicetree cause the linux  startup problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 506 views
  • Users 0 members are here
Related

when using AXI DMA,the devicetree cause the linux  startup problem

e14 Contributor
e14 Contributor over 10 years ago

Hello,everyone!
In my project,I have used a AXI DMA ip in vivado v2015.4,then created dts and devicetree.dtb.When I put devicetree.dtb in the SD Card and start linux(version is linux-xlnx-xilinx-v2015.4.01),the linux stuck in "dma-pl330 f8003000.ps7-dma:     DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16".And I have tried to change the  register address from the auto address 0x40400000 to 0x41200000 and 0x78000000,but still not working. I have no idea on it,can anyone help me?

Thanks a lot!

  • Sign in to reply
  • Cancel
  • albertabeef
    0 albertabeef over 10 years ago

    Hello,

    Here is what I would check:

    - verify that the base address in the hardware design corresponds to the base address in the device tree

    - verify that this is the core causing the crash/hang ... comment out the core in the device tree to confirm that linux boots OK

    - verify the clock source for the core ... is the clock active at the time the core is initialized ?  will the core hang is there is no clock ?

    Hope these ideas help,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to albertabeef

    Thanks very much!

    First,I have check that the hardware address is the same as in the device tree.

    Second,when comment out the core in the device tree linux boots OK.

    Third,I have used the PL Fabric clock FCLK_CLK0 100MHz for the core,is it any problem?