Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Linux Application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 1046 views
  • Users 0 members are here
Related

Linux Application

e14 Contributor
e14 Contributor over 14 years ago


I want to make an application that will run on the linux that came with the zedboard.  Can I design it and compile it using the Xilinx SDK?  Then copy the executable over to the linux?  Or do I somehow have to get the compiler and arm toolchain on that linux somehow and compile it there?  Thanks!

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 14 years ago

    Hi xspyder,

    If you are creating a C application, you certainly can use Xilinx SDK to create, edit, manage, and debug your application.

    When creating a new Xilinx C Project in SDK, make sure that you set the Software Platform option to Linux.  This will build your application using the arm-xilinx-linux-gnueabi- tools.

    You can copy the executable over to Linux by copying to the SD card, FTP, SCP, or using the SDK Remote System Explorer (RSE).

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 14 years ago

    Hi xspyder,

    If you are creating a C application, you certainly can use Xilinx SDK to create, edit, manage, and debug your application.

    When creating a new Xilinx C Project in SDK, make sure that you set the Software Platform option to Linux.  This will build your application using the arm-xilinx-linux-gnueabi- tools.

    You can copy the executable over to Linux by copying to the SD card, FTP, SCP, or using the SDK Remote System Explorer (RSE).

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to zedhed

    I am trying to get a simple Hello World app to run in linux.  I was able to successfully compile the ELF file in the SDK and upload it to linux that came with the zedboard.  It worked fine.  I then tried the same thing with xillinux (Ubuntu 12 LTS) and the ELF won't execute.  I get the following:

    root@localhost:/apps# ./Test.elf

    bash: ./Test.elf: No such file or directory


    Here is what I get when I use the file command:

    root@localhost:/apps# file Test.elf

    Test.elf: ELF 32-bit LSB executable, ARM, version 1 (SYSV), dynamically linked (uses shared libs), for GNU/Linux 2.6.16, not stripped

    root@localhost:/apps# ldd Test.elf
            not a dynamic executable


    I also did chmod +x Test.elf and that did not work.  Could it be the different kernels?  Ubuntu is running 3.3 and that file looks to be built for 2.6.16.

    Any ideas?