Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Linux Application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 1044 views
  • Users 0 members are here
Related

Linux Application

e14 Contributor
e14 Contributor over 14 years ago


I want to make an application that will run on the linux that came with the zedboard.  Can I design it and compile it using the Xilinx SDK?  Then copy the executable over to the linux?  Or do I somehow have to get the compiler and arm toolchain on that linux somehow and compile it there?  Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hi,

    I suggest compiling your application in Xillinux (using gcc). Odds are that it will work on any distribution running Linux.

    If the executable happens to depend on a library that exists on Xillinux, but on the target distribution, you may use the "-static" flag to tell gcc to generate a self-contained executable. The executable will be bigger, but this is usually a small penalty when it's a single program compiled this way.

    I've never tried to use Xilinx' SDK for this, but I take Kevin's word for that it's possible, of course.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I'm using a Windows 7 PC with SDK and I have built several elf files and I have multiple ways to install them in a directory on the Zynq.  I've tried a few hours, set the X flag etc, but I can't figure out how to get them to execute on the board.  The only discussions I can find give vague discussions how someone could write some app to then cause an elf file to be executed.   My Zynq board powers up in some version of Linux, but it is not Petalinux and does not seem to have a TCF host - so I can't seem to run it from a remote debugger either.  Please help me figure something out before I start to look like an idiot to the bean counters.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I'm using a Windows 7 PC with SDK and I have built several elf files and I have multiple ways to install them in a directory on the Zynq.  I've tried a few hours, set the X flag etc, but I can't figure out how to get them to execute on the board.  The only discussions I can find give vague discussions how someone could write some app to then cause an elf file to be executed.   My Zynq board powers up in some version of Linux, but it is not Petalinux and does not seem to have a TCF host - so I can't seem to run it from a remote debugger either.  Please help me figure something out before I start to look like an idiot to the bean counters.