Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Problem in creating dump file in VIVADO project
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 784 views
  • Users 0 members are here
Related

Problem in creating dump file in VIVADO project

e14 Contributor
e14 Contributor over 12 years ago

I had a problem in creating FILE pointer like FILE *fp; and then i opend a file like
fp = fopen("c:/user/xilinx/project1/hello.txt","w");
and i didn't get any address in file pointer while debugging and i didn't get any dump file hello.txt in my project1 help me!!!!!!!!!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Assuming that you are attempting to program a Zynq device on something like a Zedboard, you need to first understand the embedded system you are working with. Programming on the Zynq is not the same as writing a C program to run under Windows on your PC. The statement you have listed above assumes that there is a "C:" hard drive available to the system (C: is on your host PC, not on the ZedBoard), and that you have a file system implemented on the "C" drive, and that you have an operating system, like Windows, that  supports the 'fopen' operation.

     

    On a ZedBoard there is only the RAM memory internal to the Zynq device, the DDR3 DRAM, the SD Card (if installed) and the QSPI Flash device, no 'C' hard drive. Then, to perform a file operation on one of these available memory resources, you would need to implement an Operating System (such as Linux, PetaLinux, FreeRTOS, etc.) or at least one of the file system libraries (xilmfs).

     

    I suggest that you study to familiarize yourself with the Zynq system by using the resources referred to the answer to one of your previous posts: http://www.zedboard.org/content/helloworldelf-storage-location-zedboard

     

    Then perhaps move on to the PetaLinux Speedway material available at the same page pointed to for the Zynq Software and Hardware Speedway material or some other resources for embedded systems.

     

    Also, please do not continue to make duplicate posts of the same question on multiple forums.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thank you for your information. In my zedboard bootable system from SD card. How can i see the .elf from file system using teraterm window