Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Difference between ss and SPISEL in the XSPI
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 915 views
  • Users 0 members are here
Related

Difference between ss and SPISEL in the XSPI

e14 Contributor
e14 Contributor over 13 years ago

Good Day

I am working with ZEDBOARD ,I want to use AXI Xspi as a slave ,I don't know the difference between SS and SPISEL .which one should I use as chip select ?.


Thanks in advance
Jassim 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi Joe,

    You don't say what version of the tools you are using. I started with ISE 14.4 and connected through the EMIO ports. I just check the MIO ports and you're lucky. They are in the correct pin order to connect the pMod SPI device.
    JE1 A6 MIO-13 SS
    JE2 G7 MIO-10 MOSI
    JE3 B4 MIO-11 MISO
    JE4 C5 MIO-12 CLK
    The bad news is that I had to debug the spips library. The library from ISE 14.6 might work better. I copied the library routines to my own source directory and then modified them. I have submitted my changes to Xilinx and the indication is that they will be included in ISE 14.7.
    That being said, the routines in the 14.6 library are probably good enough for what you need to do. I was implementing features that the library didn't support yet.

    Good Luck,
    Mike

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi Joe,

    You don't say what version of the tools you are using. I started with ISE 14.4 and connected through the EMIO ports. I just check the MIO ports and you're lucky. They are in the correct pin order to connect the pMod SPI device.
    JE1 A6 MIO-13 SS
    JE2 G7 MIO-10 MOSI
    JE3 B4 MIO-11 MISO
    JE4 C5 MIO-12 CLK
    The bad news is that I had to debug the spips library. The library from ISE 14.6 might work better. I copied the library routines to my own source directory and then modified them. I have submitted my changes to Xilinx and the indication is that they will be included in ISE 14.7.
    That being said, the routines in the 14.6 library are probably good enough for what you need to do. I was implementing features that the library didn't support yet.

    Good Luck,
    Mike