Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development 'arm-xilinx-linux-gnueabi-gcc' is not recognized
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 1496 views
  • Users 0 members are here
Related

'arm-xilinx-linux-gnueabi-gcc' is not recognized

e14 Contributor
e14 Contributor over 13 years ago

Hi,

Iu2019m going through the CTT section 5.4.1, step 19 and I am running into an error. I am running xilinux, not the linux version used in the tutorial. Have you encounter this error before?

**** Build of configuration Debug for project leds_switches ****

make all
Building file: ../leds_switches.c
Invoking: ARM Linux gcc compiler
arm-xilinx-linux-gnueabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -MMD -MP -MF"leds_switches.d" -MT"leds_switches.d" -o"leds_switches.o" "../leds_switches.c"
'arm-xilinx-linux-gnueabi-gcc' is not recognized as an internal or external command,
operable program or batch file.
make: *** [leds_switches.o] Error 1


I read online that you should install embedded edition, but that has not helped.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    The same distribution disk image that installs a perfectly working system in Windows 7 (32-bit) has multiple problems in Linux, Xubuntu 12.10. Re-installing, I then lost EDK functionality also. It now reports an unspecified internal problem and bombs out without exporting the hardware. The installation in Windows, however, works without any glitches. The only problem is a Linux host is required for driver development. It seems they don't want us to build real systems with their tools.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    The same distribution disk image that installs a perfectly working system in Windows 7 (32-bit) has multiple problems in Linux, Xubuntu 12.10. Re-installing, I then lost EDK functionality also. It now reports an unspecified internal problem and bombs out without exporting the hardware. The installation in Windows, however, works without any glitches. The only problem is a Linux host is required for driver development. It seems they don't want us to build real systems with their tools.