Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development 'arm-xilinx-linux-gnueabi-gcc' is not recognized
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 1496 views
  • Users 0 members are here
Related

'arm-xilinx-linux-gnueabi-gcc' is not recognized

e14 Contributor
e14 Contributor over 13 years ago

Hi,

Iu2019m going through the CTT section 5.4.1, step 19 and I am running into an error. I am running xilinux, not the linux version used in the tutorial. Have you encounter this error before?

**** Build of configuration Debug for project leds_switches ****

make all
Building file: ../leds_switches.c
Invoking: ARM Linux gcc compiler
arm-xilinx-linux-gnueabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -MMD -MP -MF"leds_switches.d" -MT"leds_switches.d" -o"leds_switches.o" "../leds_switches.c"
'arm-xilinx-linux-gnueabi-gcc' is not recognized as an internal or external command,
operable program or batch file.
make: *** [leds_switches.o] Error 1


I read online that you should install embedded edition, but that has not helped.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Starting xsdk from planAhead and from the bash command line (after sourcing the appropriate settings.sh) produces the same error result.

    /usr/bin/arm-linux-gnueabi-gcc exists, but I am uncertain of its origins.

    /usr/bin/arm-linux-gnueabi-gcc -v produces the following. The reference to Ubuntu/Linaro causes me some concern that this is not the right compiler for the Zedboard's Zynq.

    Using built-in specs.
    COLLECT_GCC=arm-xilinx-linux-gnueabi-gcc
    COLLECT_LTO_WRAPPER=/usr/lib/gcc/arm-linux-gnueabi/4.7/lto-wrapper
    Target: arm-linux-gnueabi
    Configured with: ../src/configure -v --with-pkgversion='Ubuntu/Linaro 4.7.2-1ubuntu1' --with-bugurl=file:///usr/share/doc/gcc-4.7/README.Bugs --enable-languages=c,c++,go,fortran,objc,obj-c++ --prefix=/usr --program-suffix=-4.7 --enable-shared --enable-linker-build-id --with-system-zlib --libexecdir=/usr/lib --without-included-gettext --enable-threads=posix --with-gxx-include-dir=/usr/arm-linux-gnueabi/include/c++/4.7.2 --libdir=/usr/lib --enable-nls --enable-clocale=gnu --enable-libstdcxx-debug --enable-libstdcxx-time=yes --enable-gnu-unique-object --disable-libitm --enable-plugin --enable-objc-gc --enable-multilib --disable-sjlj-exceptions --with-arch=armv5t --with-float=soft --disable-werror --enable-checking=release --build=i686-linux-gnu --host=i686-linux-gnu --target=arm-linux-gnueabi --program-prefix=arm-linux-gnueabi- --includedir=/usr/arm-linux-gnueabi/include --with-headers=/usr/arm-linux-gnueabi/include --with-libs=/usr/arm-linux-gnueabi/lib
    Thread model: posix
    gcc version 4.7.2 (Ubuntu/Linaro 4.7.2-1ubuntu1)

    ==============
    It would be a simple matter to add the right soft link if it is the right compiler. At the same time, I note that arm-xilinx-eabi-gcc, the bare-metal compiler, is also missing and cannot find its headers when I try to soft-link to that same image.

    What's missing? How do I fix the software build?

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I'm guessing the initial Xilinx install failed to complete the installation for the toolchains. I don't recall whether the scripts were run as sudo or otherwise. It certainly could not have succeeded in updating /usr/bin, /usr/lib and others without root perms.

    Also, I'm assuming the bare-metal toolchain is Codesourcery Lite, which would have failed to install using the defaulted /bin/dash shell for /bin/sh.

    I'll try reinstalling everything with some fixes before commenting further... I seem to recall seeing a post with these and other installer foibles spelled out. It would be handy if that could be made sticky and prominent.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    I'm guessing the initial Xilinx install failed to complete the installation for the toolchains. I don't recall whether the scripts were run as sudo or otherwise. It certainly could not have succeeded in updating /usr/bin, /usr/lib and others without root perms.

    Also, I'm assuming the bare-metal toolchain is Codesourcery Lite, which would have failed to install using the defaulted /bin/dash shell for /bin/sh.

    I'll try reinstalling everything with some fixes before commenting further... I seem to recall seeing a post with these and other installer foibles spelled out. It would be handy if that could be made sticky and prominent.