Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development 'arm-xilinx-linux-gnueabi-gcc' is not recognized
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 1494 views
  • Users 0 members are here
Related

'arm-xilinx-linux-gnueabi-gcc' is not recognized

e14 Contributor
e14 Contributor over 13 years ago

Hi,

Iu2019m going through the CTT section 5.4.1, step 19 and I am running into an error. I am running xilinux, not the linux version used in the tutorial. Have you encounter this error before?

**** Build of configuration Debug for project leds_switches ****

make all
Building file: ../leds_switches.c
Invoking: ARM Linux gcc compiler
arm-xilinx-linux-gnueabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -MMD -MP -MF"leds_switches.d" -MT"leds_switches.d" -o"leds_switches.o" "../leds_switches.c"
'arm-xilinx-linux-gnueabi-gcc' is not recognized as an internal or external command,
operable program or batch file.
make: *** [leds_switches.o] Error 1


I read online that you should install embedded edition, but that has not helped.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Reinstalling 14.5 by hiding the old installation and re-running xsetup solved the build issues with the SDK. Apparently the Codesourcery installer failed for the initial installation.

    The CodeSourcery website makes note that Ubuntu installations typically link /bin/sh to /bin/dash, which causes problems for its installer. Point this to /bin/bash instead.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Reinstalling 14.5 by hiding the old installation and re-running xsetup solved the build issues with the SDK. Apparently the Codesourcery installer failed for the initial installation.

    The CodeSourcery website makes note that Ubuntu installations typically link /bin/sh to /bin/dash, which causes problems for its installer. Point this to /bin/bash instead.