Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development UART Interrupt
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 365 subscribers
  • Views 1686 views
  • Users 0 members are here
Related

UART Interrupt

e14 Contributor
e14 Contributor over 12 years ago

Hello everybody

I have read the xuartps.h. It is written that we can enable which interrupt by setting the interrupt mask according to this condition:
- A change in the modem signals
- Data in the receive FIFO for a configurable time without receiver activity
- A parity error
- A framing error
- An overrun error
- Transmit FIFO is full
- Transmit FIFO is empty
- Receive FIFO is full
- Receive FIFO is empty
- Data in the receive FIFO equal to the receive threshold

I got example from Xilinx SDK. The interrupt mask can be set as:
IntrMask = XUARTPS_IXR_TOUT | XUARTPS_IXR_PARITY | XUARTPS_IXR_FRAMING | XUARTPS_IXR_OVER | XUARTPS_IXR_TXEMPTY | XUARTPS_IXR_RXFULL | XUARTPS_IXR_RXOVR;

But when I change it to:
IntrMask = XUARTPS_IXR_TOUT | XUARTPS_IXR_RXFULL | XUARTPS_IXR_RXOVR;

The program is still interrupted when I send something to the uart using XUartPs_Send.

Can anybody hep me? Thanks before

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Can anyone help? thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 12 years ago

    Hi dicksigmund,

    Have you checked to see what the actual source of the interrupt is?

    I see you have the receive timeout interrupt enabled by XUARTPS_IXR_TOUT.  By enabling this, you should get an interrupt when the receiver does not receive a new character within the timeout period set in Rcvr_timeout_regX. 

    According to UG585, Register Rcvr_timeout_reg0 Details:

    "The read/write Receiver Timeout register is used to enable the UART to detect an idle condition on the
    receiver data line. The timeout value (RTO) indicates the maximum delay for which the UART should wait
    for a new character to arrive before issuing a timeout interrupt."

    Could you be seeing this interrupt occur during your XUartPs_Send()?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I have checked the actual source of interrupt by using event checking in my handler:
    if (Event == XUARTPS_EVENT_SENT_DATA) {
    txil_printf("Ar
    ");
    }

    In my main program, I send a character by using:
    XUartPs_Send(&UartPs, "test", 4);

    The console printed out: testA

    Thus, I concluded that the interrupt still occurred when I send something via UART. Is there anything wrong with my method in defining the Interrupt Mask?

    Thank you very much for your reply, Kevin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fayyazrafiq
    0 fayyazrafiq over 12 years ago in reply to e14 Contributor

    Hi

    First thing, do not use time out interrupt on receiver. Second thing is remove the printf, because it is not preferable to use printf statement in ISR. Use send method only. One more thing which i observed, you are sending data from two places 1) one from main using send method and one from ISR using printf. This can cause data corruption, So only use send in ISR and send only one byte and see whether you are still getting interrupt or not. I hope, this will work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Thank you very much, fayyazrafiq. It works now. I have fixed it