Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Ultrazed: SD card booting failure
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 364 subscribers
  • Views 1101 views
  • Users 0 members are here
Related

Ultrazed: SD card booting failure

e14 Contributor
e14 Contributor over 9 years ago

Hello, 

I'm trying to boot a petalinux from the SD card without any success. I have tried the one provided by avnet or one that I build with petalinux + vivado (I tried both 2016.2 and 2016.4).

The system is  booting on the EMMC and not with the uImage of the SD card...

 

With the one provided by avnet I have the following problem:

*** Warning - spi_flash_probe() failed, using default environment

With mine I have the following error:

*** Warning - bad CRC, using default environment

Do you have some suggestions?
Thanks
  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello simalps,

    This seems quite strange you are encountering an issue with the provided SD boot.bin file. Just so I understand and have all the details, you are following the UltraZed-EG Starter Kit Tutorial correct http://zedboard.org/support/design/14201/126 ?

    Are you using the SD card that came with your kit or a different one? If you are using a different one is it formatted to FAT or FAT32(also please provide what kind of SD card you have back to me)? And for a sanity check , please double check you are setup correctly for SD Card boot(SOM SW2 Boot Mode switch (MODE[3:0] = SW2[4:1]) to ON, OFF, ON, and OFF positions (Boot Mode set to SD Card, MODE[3:0] = 0x5))

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello simalps,

    This seems quite strange you are encountering an issue with the provided SD boot.bin file. Just so I understand and have all the details, you are following the UltraZed-EG Starter Kit Tutorial correct http://zedboard.org/support/design/14201/126 ?

    Are you using the SD card that came with your kit or a different one? If you are using a different one is it formatted to FAT or FAT32(also please provide what kind of SD card you have back to me)? And for a sanity check , please double check you are setup correctly for SD Card boot(SOM SW2 Boot Mode switch (MODE[3:0] = SW2[4:1]) to ON, OFF, ON, and OFF positions (Boot Mode set to SD Card, MODE[3:0] = 0x5))

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Hello Josh,

    I confirm that jumpers are well configured to 0x5. I made additional tests. I already tried the files provided by the link you posted. Both are not working.

    I have now tried to build the BSP and the image using the official Avnet script: https://github.com/Avnet/software/blob/master/petalinux/scripts/make_uz3eg_petalinux_bsp.sh using this one seems to work but I still have the same error during the booting procedure. However, the petalinux OOB release is the 1.1 (instead of the 1.0) and I can see a dummy application that I introduced during the petalinux build.

    Creating my own petalinux does not work. I followed this steps

    petalinux-create --type project --template zynqMP --name zynqmptest

    cd zynqmptest

    petalinux-config --get-hw-description=<here I tried with both a project created from scratch and one from the bsp script>

    petalinux-create -t apps  --name dummyapp --enable

    petalinux-build

    petalinux-package --boot --format BIN --fsbl zynqmp_fsbl.elf --fpga design_1_wrapper.bit --u-boot --force

     

    This does not works.