Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Ultrazed: SD card booting failure
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 364 subscribers
  • Views 1099 views
  • Users 0 members are here
Related

Ultrazed: SD card booting failure

e14 Contributor
e14 Contributor over 9 years ago

Hello, 

I'm trying to boot a petalinux from the SD card without any success. I have tried the one provided by avnet or one that I build with petalinux + vivado (I tried both 2016.2 and 2016.4).

The system is  booting on the EMMC and not with the uImage of the SD card...

 

With the one provided by avnet I have the following problem:

*** Warning - spi_flash_probe() failed, using default environment

With mine I have the following error:

*** Warning - bad CRC, using default environment

Do you have some suggestions?
Thanks
  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello simalps,

    Just to double check, JP1 on the IO carrier card has a jumper installed correct?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Hello Josh,

    thanks for your reply.

    Yes, it has: JP1 on the IO carrier card is armed. I tried to remove it and I also tried to arm the JP2 on the IO carrier card without any success. (Actually. I tried all the permutations of JP1 and JP2).

    JP1 of the SOM has been removed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Hello Josh,

    thanks for your reply.

    Yes, it has: JP1 on the IO carrier card is armed. I tried to remove it and I also tried to arm the JP2 on the IO carrier card without any success. (Actually. I tried all the permutations of JP1 and JP2).

    JP1 of the SOM has been removed.