Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development MM2S simple transfer gone wrong
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 362 subscribers
  • Views 221 views
  • Users 0 members are here
Related

MM2S simple transfer gone wrong

jmales
jmales over 11 years ago

I followed some examples and I already managed to make a big S2MM (stream to memory-mapped) transfer via an AXI DMA (http://www.xilinx.com/support/documentation/ip_documentation/axi_dma/v7_1/pg021_axi_dma.pdf).

However, now I'm trying the reverse, i.e. to make a simple MM2S transfer to a very simple IP block that I made and the result returned from the block is wrong. Note that the MM2S code is also almost a copy from examples that I found.

I tried debugging with the ILA(integrated Logic Analyzer) tool from Vivado and the result is in attachement.

Can you help me understand why I'm writing the following values:

static void initialize_parameters(u32 SrcAddress){
u32 *BufferPtr;
union float32 thisfloat;

BufferPtr=(u32*)(SrcAddress);
thisfloat.f32=10.0;
BufferPtr[0]=thisfloat.u32;

thisfloat.f32=0.0;
BufferPtr[1]=thisfloat.u32;

thisfloat.f32=10.0;
BufferPtr[2]=thisfloat.u32;

thisfloat.f32=20.0;
BufferPtr[3]=thisfloat.u32;

}

and making a transfer like this:

// Kick off DMA transfers
Status = XAxiDma_SimpleTransfer(&axi_dma, PARAMETERS_ADDR, 4*4, XAXIDMA_DMA_TO_DEVICE);

and the signal parameters_TDATA when tvalid=1 is that thing that we can see in attachement? Also, the final result is incorrect. What am I doing wrong?
http://postimg.org/image/rnt7yc58v/

Also, here's a print screen of my block design in Vivado. Note: I'm working on a Zedboard
http://postimg.org/image/gi7nbfa0l/