Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development MicroZed Bare Metal LWIP Multicast receiver
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 365 subscribers
  • Views 1145 views
  • Users 0 members are here
Related

MicroZed Bare Metal LWIP Multicast receiver

e14 Contributor
e14 Contributor over 11 years ago

Hello,

Would you please help me ?

I am trying to run the LWIP Multicast Receiver application on MicroZed board in Bare Metal mode.

Previously, I tested TCP-IP and UDP-IP cases with success.

Below is the entire code of the multicast application, followed by a screen capture.
Sorry, it's a little bit long.

Please, tell me what's wrong ?

#include <stdio.h>

#include "xscugic.h"

#include <xil_io.h>
#include "netif/xadapter.h"
#include "lwip/udp.h"
#include "xstatus.h"
#include "lwip/err.h"

#include "lwip/igmp.h"


/* missing declaration in lwIP */
extern "C"
{
void lwip_init();
}

/* The instance of the netif Server based on Eth_0 */
static struct netif gs_netifUdpIpMulticastEth_0;

/* The Instance of the Interrupt Controller Driver */
static XScuGic gs_xScuGic;

/* PORT NUMBER */
unsigned int gsc_uiPortNumber(45454);

/* The instance of the udp pcb for multicast */
struct udp_pcb * g_aUdpPcb(0);

// Callback for UDP multicast receiving datagrams
static void UdpReceiverRoutine(void *arg, struct udp_pcb *pcb, struct pbuf *p, ip_addr_t *addr, u16_t port)
{
tstruct pbuf * qbuf(p);
tu8 u8NumBufInQueue(1);
  printf("Receive datagram
r");
tif (p)
t{
tt// Here, payload is a "C string" with 0 sized
ttprintf("Received datagram frag : 001
r");
tt//printf("Received datagram n: 001 :
r%s
r", (char*) qbuf->payload);
ttfflush(stdout);

ttwhile (qbuf->next != NULL)
tt{
tttprintf("Received datagram frag : %03u
r", (unsigned int)u8NumBufInQueue);
ttt//printf("Received datagram n: %03u :
r%s
r", (unsigned int)u8NumBufInQueue, (char*) qbuf->payload);
tttfflush(stdout);

tttu8NumBufInQueue++;
tt}

ttpbuf_free(p);
t}
}

/****************************************************************************/
/**
* This function sets up the interrupt system.  The processing
* contained in this function assumes the hardware system was built with
* and interrupt controller.
*
* @paramtNone.
*
* @returntA status indicating XST_SUCCESS or a value that is contained in
*ttxstatus.h.
*
* @notettNone.
*
*****************************************************************************/
int SetupInterruptSystem(XScuGic * const aXScuGic)
{
t/* Initialize the interrupt controller driver so that it is ready to use.
t */
tXScuGic_Config * const aXScuGic_Config(XScuGic_LookupConfig(XPAR_PS7_SCUGIC_0_DEVICE_ID));
tif (aXScuGic_Config == NULL)
ttreturn XST_FAILURE;

tif (XScuGic_CfgInitialize(aXScuGic, aXScuGic_Config, aXScuGic_Config->CpuBaseAddress) != XST_SUCCESS)
ttreturn XST_FAILURE;

t/* Connect the interrupt controller handler to the hardware
t * interrupt handling logic in the ARM processor
t */
tXil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_INT, (Xil_ExceptionHandler)XScuGic_InterruptHandler, aXScuGic);

t/* Initialize the exception table and register the interrupt
t * controller handler with the exception table
t */
tXil_ExceptionInit();

t/* Enable non-critical exceptions in the ARM
t */
tXil_ExceptionEnable();


treturn XST_SUCCESS;
}

/*****************************************************************************/
/**
* Setup multicast configuration
*
* Group addr : 234.6.6.6
* Port : 45454
* MAC software coded but fixed for MicroZed Evaluation Board :
*            00:0a:35:00:01:02
*****************************************************************************/
int SetupUdpIpMulticastEth_0(struct netif * const aNetif)
{
tstruct ip_addr ipaddr, netmask, gw;
tstruct ip_addr ipgroup; // for multicast
terr_t err;

t/*
t * The mac address of the board.
t * !!! Take care with MicroZed board. This should be unique per board
t * */
tunsigned char s_ucMac_EthernetArray[] = {
t    0x00, 0x0a, 0x35, 0x00, 0x01, 0x02 };

t/*
t * Initialize IP addresses to be used
t */
tIP4_ADDR(&ipaddr, 192, 168, 1, 10);
tIP4_ADDR(&netmask, 255, 255, 255, 0);
tIP4_ADDR(&gw, 192, 168, 1, 1);
tIP4_ADDR(&ipgroup, 234, 6, 6, 6);

t/*
t * Initialize the Light Weight Internet Protocol library
t */
t/////////////////////////////////////////////////////////////////////////////
tlwip_init(); // Also calls igmp_init() function
t/////////////////////////////////////////////////////////////////////////////


t/*
t * Add network interface to the netif_list, and set it as default
t *
t * Also calls igmp_start(...) function
t **/
tif (!xemac_add(aNetif, &ipaddr, &netmask, &gw, s_ucMac_EthernetArray,
tXPAR_XEMACPS_0_BASEADDR))
t{
ttprintf("Error adding N/W interface
r");
ttreturn -1;
t}

t//////////////////////////////////////////////////////////////
tnetif_set_default(aNetif);
t//////////////////////////////////////////////////////////////

t/*
t * Set the network up
t */
t//////////////////////////////////////////////////////////////
tnetif_set_up(aNetif);
t//////////////////////////////////////////////////////////////

t/*
t * Create new UDP PCB structure
t */
t//////////////////////////////////////////////////////////////
tg_aUdpPcb = udp_new();
t//////////////////////////////////////////////////////////////

tif (!g_aUdpPcb)
t{
ttprintf("Error creating UDP PCB. Out of Memory
r");
ttreturn -1;
t}

t/*
t * Bind to specified port
t */
t////////////////////////////////////////////////////////////////////////////
terr = udp_bind(g_aUdpPcb, IP_ADDR_ANY, gsc_uiPortNumber);
t////////////////////////////////////////////////////////////////////////////

tif (XST_SUCCESS != err)
t{
ttprintf("Unable to bind to port %d: err = %d
r", gsc_uiPortNumber, err);
ttreturn err;
t}


t////////////////////////////////////////////////////////////////////////////
terr = igmp_joingroup(IP_ADDR_ANY, &ipgroup);
t////////////////////////////////////////////////////////////////////////////

tif (XST_SUCCESS != err)
t{
ttprintf("
rXST_SUCCESS != igmp_joingroup(IP_ADDR_ANY, &ipgroup) : %d
r", err);
ttreturn err;
t}

t/*
t * Start UDP Receiver
t */
t////////////////////////////////////////////////////////////////////////////
tudp_recv(g_aUdpPcb, UdpReceiverRoutine, NULL);
t////////////////////////////////////////////////////////////////////////////

treturn XST_SUCCESS;
}


/******************************************************************************/
/**
* main
*
*******************************************************************************/
//volatile CmsVideoSs::Sap sap;
int main()
{
tint iStatus;

txil_printf("Hello world
r");

t/* Setup the interrupts such that interrupt processing can occur.
t * If an error then exit
t */
txil_printf("SetupInterruptSystem(&gs_xScuGic) : ");
tif (XST_SUCCESS != (iStatus = SetupInterruptSystem(&gs_xScuGic)))
t{
ttxil_printf("FAILED
r");
ttreturn iStatus;
t}
telse
t{
ttxil_printf("PASSED
r");
t}

t/* Setup the UDP Multicast.
t * If an error then exit
t */
txil_printf("SetupUdpIpMulticastEth_0(&gs_netifUdpIpMulticastServerEth_0) : ");
tif (XST_SUCCESS
ttt!= (iStatus = SetupUdpIpMulticastEth_0(&gs_netifUdpIpMulticastEth_0)))
t{
ttxil_printf("FAILED
r");
ttreturn iStatus;
t}
telse
t{
ttxil_printf("PASSED
r");
t}

t// Main loop
twhile (1)
t{

ttxemacif_input(&gs_netifUdpIpMulticastEth_0);
t}

treturn XST_SUCCESS;
}

// SCREEN CAPTURE
Hello world
SetupInterruptSystem(&gs_xScuGic) : PASSED
SetupUdpIpMulticastEth_0(&gs_netifUdpIpMulticastServerEth_0) : igmp_init: initializing
Start PHY autonegotiation
Waiting for PHY to complete autonegotiation.
autonegotiation complete
link speed: 100
pbuf_alloc(length=1518)
pbuf_alloc: allocated pbuf 0x1bc868
pbuf_alloc(length=1518) == 0x1bc868
pbuf_alloc(length=1518)
...
pbuf_alloc: allocated pbuf 0x1a1668
pbuf_alloc(length=1518) == 0x1a1668
pbuf_alloc(length=1518)
pbuf_alloc: allocated pbuf 0x1a0f68
pbuf_alloc(length=1518) == 0x1a0f68
igmp_start: starting IGMP processing on if 0x128238
igmp_lookup_group: allocated a new group with address 224.0.0.1 on if 0x128238
igmp_start: igmp_mac_filter(ADD 224.0.0.1) on if 0x128238
pbuf_alloc(length=42)
pbuf_alloc(length=42) == 0x128840
pbuf_free(0x128840)
pbuf_free: 0x128840 has ref 1, ending here.
pbuf_free: 0x128840 pbuf_free: deallocating 0x128840
igmp_report_groups: sending IGMP reports on if 0x128238
udp_bind(ipaddr = 0.0.0.0, port = 45454)
udp_bind: bound to 0.0.0.0, port 45454
igmp_lookup_group: allocated a new group with address 234.6.6.6 on if 0x128238
igmp_joingroup: join to new group: 234.6.6.6
igmp_joingroup: igmp_mac_filter(ADD 234.6.6.6) on if 0x128238
pbuf_alloc(length=8)
pbuf_alloc(length=8) == 0x128840
pbuf_header: old 0x1288c0 new 0x1288bc (4)
pbuf_header: old 0x1288bc new 0x1288a8 (20)
ip_output_if: te0
IP header:
+-------------------------------+
| 4 | 6 |  0x00 |        32     | (v, hl, tos, len)
+-------------------------------+
|        0      |000|       0   | (id, flags, offset)
+-------------------------------+
|    1  |    2  |    0x0000     | (ttl, proto, chksum)
+-------------------------------+
|  192  |  168  |    1  |   10  | (src)
+-------------------------------+
|  234  |    6  |    6  |    6  | (dest)
+-------------------------------+
netif->output()pbuf_header: old 0x1288a8 new 0x12889a (14)
pbuf_free(0x128840)
pbuf_free: 0x128840 has ref 1, ending here.
pbuf_free: 0x128840 pbuf_free: deallocating 0x128840
PASSED
pbuf_alloc(length=1518)
pbuf_alloc: allocated pbuf 0x1a0868
pbuf_alloc(length=1518) == 0x1a0868
pbuf_alloc(length=1518)
pbuf_alloc: allocated pbuf 0x1a0168
pbuf_alloc(length=1518) == 0x1a0168
pbuf_header: old 0x1bc8c0 new 0x1bc8ce (-14)
ip_input: iphdr->dest 0xff01a8c0 netif->ip_addr 0xa01a8c0 (0x1a8c0, 0x1a8c0, 0xff000000)
ip_input: packet accepted on interface te
ip_input:
IP header:
+-------------------------------+
| 4 | 5 |  0x00 |        36     | (v, hl, tos, len)
+-------------------------------+
|    27014      |000|       0   | (id, flags, offset)
+-------------------------------+
|  128  |   17  |    0x4c8f     | (ttl, proto, chksum)
+-------------------------------+
|  192  |  168  |    1  |  100  | (src)
+-------------------------------+
|  192  |  168  |    1  |  255  | (dest)
+-------------------------------+



  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Alexmoran,

    Unfortunatly we do not have much expertise in this area. I would suggest you go and ask this question over at the xilinx forum.

    https://forums.xilinx.com/

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Alexmoran,

    Unfortunatly we do not have much expertise in this area. I would suggest you go and ask this question over at the xilinx forum.

    https://forums.xilinx.com/

    --Josh