Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development transfer data from PS to PL on linux Platform
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 793 views
  • Users 0 members are here
Related

transfer data from PS to PL on linux Platform

shivangi_29
shivangi_29 over 8 years ago

There is a zynq processor and custom IP, interconnection between these two are through AXI interconnect bridge. I have created devicetree.dtb file..Now next step is to transfer data through AXI. I get to know we can do it through UIO method but dont know how to start. 
I have done some changes in .dtb file and UIO0 has been created in /dev/uio0. There is also two mapping shown in /sys/class/uio/maps/mapo/map1. 

This is my .dtb file

 PL.dts

 

 {

amba_pl: amba_pl {

#address-cells = <1>;

#size-cells = <1>;

compatible = "simple-bus";

ranges ;

mod_ip_0: mod_ip@43c00000 {

compatible = "dmen-uio";

reg = <0x43c00000 0x10000 0x7aa00000 0x10000>;

xlnx,s00-axi-addr-width = <0x4>;

xlnx,s00-axi-data-width = <0x20>;

xlnx,s01-axi-addr-width = <0xa>;

xlnx,s01-axi-aruser-width = <0x1>;

xlnx,s01-axi-awuser-width = <0x1>;

xlnx,s01-axi-buser-width = <0x1>;

xlnx,s01-axi-data-width = <0x20>;

xlnx,s01-axi-id-width = <0xc>;

xlnx,s01-axi-ruser-width = <0x1>;

xlnx,s01-axi-wuser-width = <0x1>;

};

};

};

 

C coding:

ad9361_uio_fd = open(AD9361_UIO_DEV, O_RDWR);

printf("hi");

if(ad9361_uio_fd < 1)

{

printf("%s: Can't open ad9361_uio device\n\r", __func__);

return;

}

 

 

 

FILE *fp;

uint32_t mem_size=0x10000;

uint32_t mem_addr=0x43c00000;

fp = fopen ("/sys/class/uio/uio0/maps/map0/size","r");

fscanf(fp,"0x%0x", &mem_size);

fclose(fp);

fp = fopen ("/sys/class/uio/uio0/maps/map0/addr","r");

fscanf(fp,"0x%0x", &mem_addr);

fclose(fp);

 

 

FILE *fs;

uint32_t mem_size_1=0x10000;

uint32_t mem_addr_1=0x7aa00000;

fs = fopen ("/sys/class/uio/uio0/maps/map1/size","r");

fscanf(fs,"0x%0x", &mem_size_1);

fclose(fs);

fs = fopen ("/sys/class/uio/uio0/maps/map1/addr","r");

fscanf(fs,"0x%0x", &mem_addr_1);

fclose(fs);

 

I am stuck at this point. what will be the next step??

Thanks

Shivangi

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello,

    What board are you running this on?

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shivangi_29
    0 shivangi_29 over 8 years ago in reply to jafoste4

    Hello

    What board are you running this on?

    Zedboard, zynq 7000 SOC IC.

    Thanks