Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development AXI Device Driver
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 550 views
  • Users 0 members are here
Related

AXI Device Driver

e14 Contributor
e14 Contributor over 13 years ago

Hi

I'm trying to write a device driver for a simple FIFO based peripheral which was generated using the "Create/Import Peripheral" wizard in XPS but it seg faults every time I try to read from it.  Writing data seems to work without any problems (I haven't Chipscoped the interconnect yet, but that's what I'm about to do).  The code in my read function is as follows:

int readData(void *address, int* data)
{
  if ((int) address == A2F_OUT_BASE)
    {
      #ifdef DEBUG
        printk(KERN_INFO "Attempting to read from phys: %p, mapped to %p
", address, out_mmio);
      #endif
      *data = ioread32(out_mmio); /* CRASH HERE */
    }
  else
    return -2;

  #ifdef DEBUG
    printk(KERN_INFO "Reading %d from %p successful.
", *data, address);
  #endif

  return SUCCESS;
}

'A2F_OUT_BASE' contains the physical address (hard coded), 'address' has the same value (I've checked), and 'data' (a kernel space pointer) should contain the data I get back; however it crashes during the ioread32.  I have previously used ioremap to map the physical address to out_mmio and this does not return 0.  As previously mentioned, I have written to the other end of the fifo  using the same technique, but with iowrite32, without a segmentation fault.

Is there something special I need to do to get the AXI to read the value, or am I doing this in entirely the wrong way?

Thanks in advance,
Matthew

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I am remapping the HW address to a virtual address using ptr = ioremap_nocache(DIRECTION,SIZE);
    were ptr, is a void pointer passed to ioread32(). Works perfect for me. I hope this help you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I am remapping the HW address to a virtual address using ptr = ioremap_nocache(DIRECTION,SIZE);
    were ptr, is a void pointer passed to ioread32(). Works perfect for me. I hope this help you.