Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Linux stop after console [tty0] enabled, bootconsole disabled
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 2245 views
  • Users 0 members are here
Related

Linux stop after console [tty0] enabled, bootconsole disabled

e14 Contributor
e14 Contributor over 12 years ago

I did a PCB by myself based on the zedboard. Except having no HDMI, Audio, button, all the others are same. I made a SD according to the instruction of www.xillybus.com. It can run on the zedboard, but after I changed to my own PCB, the linux can not run normally.It stop after console [tty0] enabled, bootconsole disabled. The followings are the output from serial port:
In:    serial
Out:   serial
Err:   serial
Net:   zynq_gem
Hit any key to stop autoboot:  0
Copying Linux from SD to RAM...
Device: SDHCI
Manufacturer ID: 3
OEM: 5344
Name: SU08G
Tran Speed: 25000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 7.4 GiB
Bus Width: 4-bit
reading zImage

2930600 bytes read
reading devicetree.dtb

6248 bytes read
reading ramdisk8M.image.gz

** Unable to read "ramdisk8M.image.gz" from mmc 0:1 **
## Starting application at 0x00008000 ...
Uncompressing Linux... done, booting the kernel.
[    0.000000] Booting Linux on physical CPU 0
[    0.000000] Linux version 3.3.0-xillinux-1.1+ (eli@ocho.localdomain) (gcc ver
sion 4.5.1 (Sourcery G++ Lite 2010.09-62) ) #1 SMP PREEMPT Thu Dec 20 20:55:07 I
ST 2012
[    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructio
n cache
[    0.000000] Machine: Xilinx Zynq Platform, model: Xillinux for Zedboard
[    0.000000] bootconsole [earlycon0] enabled
[    0.000000] Memory policy: ECC disabled, Data cache writealloc
[    0.000000] BUG: mapping for 0xf8f00000 at 0xfe00c000 out of vmalloc space
[    0.000000] BUG: mapping for 0xe0000000 at 0xfe000000 out of vmalloc space
[    0.000000] BUG: mapping for 0xffff1000 at 0xfe200000 out of vmalloc space
[    0.000000] PERCPU: Embedded 7 pages/cpu @c0a58000 s5632 r8192 d14848 u32768
[    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pag
es: 125824
[    0.000000] Kernel command line: consoleblank=0 root=/dev/mmcblk0p2 rw rootwa
it earlyprintk
[    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)
[    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
[    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
[    0.000000] Memory: 240MB 256MB = 496MB total
[    0.000000] Memory: 496820k/496820k available, 27468k reserved, 0K highmem
[    0.000000] Virtual kernel memory layout:
[    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
[    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
[    0.000000]     vmalloc : 0xe0800000 - 0xfd000000   ( 456 MB)
[    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)
[    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
[    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
[    0.000000]       .text : 0xc0008000 - 0xc054559c   (5366 kB)
[    0.000000]       .init : 0xc0546000 - 0xc0572600   ( 178 kB)
[    0.000000]       .data : 0xc0574000 - 0xc05af080   ( 237 kB)
[    0.000000]        .bss : 0xc05af0a4 - 0xc05d0778   ( 134 kB)
[    0.000000] Preemptible hierarchical RCU implementation.
[    0.000000]  Verbose stalled-CPUs detection is disabled.
[    0.000000] NR_IRQS:128
[    0.000000] xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43
[    0.000000] Console: colour dummy device 80x30
[    0.000000] console [tty0] enabled, bootconsole disabled
Would you like to help me? Thanks a lot.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    Unfortunately, the log you supplied doesn't help much, since it stops where it usually does on Xillinux-1.1: After the VGA screen starts. On a Zedboard, the rest of the log goes to the screen. I understand that you don't have any.

    I suspect that the reason is that you removed the xillyvga core from the processor's bus. If you didn't remove it from the device tree as well, Linux won't boot. Same goes for any IP core you might have removed.

    If this is not the issue, we need the full log until it gets stuck. In Xillinux-1.3 all of the log goes to the serial console, so upgrading should do the trick.

    Hope this helps,
      Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,

    Unfortunately, the log you supplied doesn't help much, since it stops where it usually does on Xillinux-1.1: After the VGA screen starts. On a Zedboard, the rest of the log goes to the screen. I understand that you don't have any.

    I suspect that the reason is that you removed the xillyvga core from the processor's bus. If you didn't remove it from the device tree as well, Linux won't boot. Same goes for any IP core you might have removed.

    If this is not the issue, we need the full log until it gets stuck. In Xillinux-1.3 all of the log goes to the serial console, so upgrading should do the trick.

    Hope this helps,
      Eli