Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Linux design boots on Zedboard, but not customer target board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 306 views
  • Users 0 members are here
Related

Linux design boots on Zedboard, but not customer target board

e14 Contributor
e14 Contributor over 12 years ago

Customer can boot Linux on Zedboard,but not on custom target board.  Note that Linux was previously booting the target board with 2013.3 and the customer decided to move to 2013.4, when this seems to have broken.  The customer is using the 2012 Linux Speedway as a reference.

It looks as if it is failing during the FSLB.  The .BIT file is not loading.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Tim,

     

    Xilinx made a change in the SD 'driver' in the 2013.4 FSBL to monitor the status of the PS SDIO WP pin. If this pin is not connected on the custom board that could be the issue. If this is the issue one potential fix is to go into the PS config and bring the SDIO WP pin out to an EMIO pin and tie it to '0' using a 'constant' IP block.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi Tim,

     

    Xilinx made a change in the SD 'driver' in the 2013.4 FSBL to monitor the status of the PS SDIO WP pin. If this pin is not connected on the custom board that could be the issue. If this is the issue one potential fix is to go into the PS config and bring the SDIO WP pin out to an EMIO pin and tie it to '0' using a 'constant' IP block.

     

    -Gary