Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development SDIO Wifi driver (AR6103) problem
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 364 subscribers
  • Views 1544 views
  • Users 0 members are here
Related

SDIO Wifi driver (AR6103) problem

e14 Contributor
e14 Contributor over 12 years ago

I am trying to use an Atheros AR6103 wifi module (SDIO interface) on the Zedboard.


As it is said on the Xilinx wiki website, the driver for the AR6103 is already part of the linux kernel,


here it is:  http://www.wiki.xilinx.com/Zynq+SDIO+WiFi  and http://wireless.kernel.org/en/users/Drivers/ath6kl.


The problem is that the wifi module comes in the forms of a SD card shape, but I have to use the SD slot on the Zedboard to boot the linux kernel.  If I use a Pmod to SD module to extend with one SD slot,  I have also to configure another SDIO controller in the PS using EMIOs to connect the Pmod.


What changes should I do if I want to use this integrated driver software in the Linux kernel ?  I know I have to regenerate the FSBL and bitstream.  What about the u-boot ? or any changes when building the linux kernel ?  Does the driver software automatically works with two SDIO controller ?


Thanks.


  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    PS: The following information are also shown on the termianl:



    mmc0: Invalid maximum block size, assuming 512 bytes
    mmc0: SDHCI controller on e0100000.ps7-sdio [e0100000.ps7-sdio] using ADMA
    mmc1: Invalid maximum block size, assuming 512 bytes
    mmc1: SDHCI controller on e0101000.ps7-sdio [e0101000.ps7-sdio] using ADMA





    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    PS: The following information are also shown on the termianl:



    mmc0: Invalid maximum block size, assuming 512 bytes
    mmc0: SDHCI controller on e0100000.ps7-sdio [e0100000.ps7-sdio] using ADMA
    mmc1: Invalid maximum block size, assuming 512 bytes
    mmc1: SDHCI controller on e0101000.ps7-sdio [e0101000.ps7-sdio] using ADMA