Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Linux Drivers for 7" Zed Touch Display Kit
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 366 subscribers
  • Views 1047 views
  • Users 0 members are here
Related

Linux Drivers for 7" Zed Touch Display Kit

e14 Contributor
e14 Contributor over 11 years ago

Are there Linux drivers available for the 7" Zed Touch Display Kit?  There is a precompiled example design called "Display Panel Ubuntu Tutorial for ZedBoard", and there is a ISE 14.4 patch file which references several header/source files located at "drivers/gpu/drm/zeddispkit/", but I haven't been able to locate these.

Any help would be greatly appreciated.

Thanks,
Greg

  • Sign in to reply
  • Cancel
  • zedhed
    0 zedhed over 11 years ago

    Hi Greg,

    Applying that patch file should add the header/source files to the kernel source tree.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    Thanks, Kevin. I didn't realize the patch included the missing files.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jothin
    0 jothin over 11 years ago in reply to zedhed

    Hi,

    The patch can be applied for xilinx_v2015.2 linux also

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • armendzh
    0 armendzh over 10 years ago

    I am trying to apply this patch to Xilinx_v2015.2.
    Some files have changed from the version 14.4 for which this patch is made. Is there an updated patch for Xilinx v2015.2 available somewhere?

    I am trying to get display kit to work with PetaLinux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • armendzh
    0 armendzh over 10 years ago in reply to armendzh

    After trying to patch PetaLinux 2015.2 using available patch from AVNET, I am getting following error or warnings when saving kernel configuration.

    ======================
    configuration written to /home/adzh/zynq_mini-itx_amp10/subsystems/linux/configs/kernel/config

    *** End of the configuration.
    *** Execute 'make' to start the build or try 'make help'.

    warning: (DRM_KMS_CMA_HELPER && DRM_RADEON && DRM_NOUVEAU && DRM_I915_FBDEV && DRM_EXYNOS && DRM_ROCKCHIP && DRM_GMA500 && DRM_UDL && DRM_AST && DRM_MGAG200 && DRM_CIRRUS_QEMU && DRM_ARMADA && DRM_RCAR_DU && DRM_SHMOBILE && DRM_OMAP && DRM_TILCDC && DRM_QXL && DRM_BOCHS && DRM_MSM_FBDEV && DRM_IMX && DRM_TEGRA_FBDEV) selects DRM_KMS_FB_HELPER which has unmet direct dependencies (HAS_IOMEM && DRM_KMS_HELPER)
    warning: (DRM_KMS_CMA_HELPER && DRM_RADEON && DRM_NOUVEAU && DRM_I915_FBDEV && DRM_EXYNOS && DRM_ROCKCHIP && DRM_GMA500 && DRM_UDL && DRM_AST && DRM_MGAG200 && DRM_CIRRUS_QEMU && DRM_ARMADA && DRM_RCAR_DU && DRM_SHMOBILE && DRM_OMAP && DRM_TILCDC && DRM_QXL && DRM_BOCHS && DRM_MSM_FBDEV && DRM_IMX && DRM_TEGRA_FBDEV) selects DRM_KMS_FB_HELPER which has unmet direct dependencies (HAS_IOMEM && DRM_KMS_HELPER)
    warning: (DRM_KMS_CMA_HELPER && DRM_RADEON && DRM_NOUVEAU && DRM_I915_FBDEV && DRM_EXYNOS && DRM_ROCKCHIP && DRM_GMA500 && DRM_UDL && DRM_AST && DRM_MGAG200 && DRM_CIRRUS_QEMU && DRM_ARMADA && DRM_RCAR_DU && DRM_SHMOBILE && DRM_OMAP && DRM_TILCDC && DRM_QXL && DRM_BOCHS && DRM_MSM_FBDEV && DRM_IMX && DRM_TEGRA_FBDEV) selects DRM_KMS_FB_HELPER which has unmet direct dependencies (HAS_IOMEM && DRM_KMS_HELPER)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • armendzh
    0 armendzh over 10 years ago

    I started looking at updating display driver for PetaLinux and mini-ITX board to be able to use AVNET touch screen display.

    I have everything updated except for display driver files. I pressume most of those errors are due to changes made to the framebuffer from the time of kernel 3.6 to kernel 3.19 (to which I am trying to update).

    Here are error I am getting when building my image:
    [code]
    ====================================================
    [ALL  ]   CC      drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.o
    [ALL  ] /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.c: In function 'zeddispkit_drm_crtc_update':
    [ALL  ] /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.c:50:35: error: 'struct drm_crtc' has no member named 'fb'
    [ALL  ]   struct drm_framebuffer *fb = crtc->fb;
    [ALL  ]                                    ^
    [ALL  ] /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.c:64:30: error: 'struct xilinx_vdma_config' has no member named 'hsize'
    [ALL  ]    zeddispkit_crtc->dma_config.hsize = mode->hdisplay * fb->bits_per_pixel / 8;
    [ALL  ]                               ^
    [ALL  ] /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.c:65:30: error: 'struct xilinx_vdma_config' has no member named 'vsize'
    [ALL  ]    zeddispkit_crtc->dma_config.vsize = mode->vdisplay;
    [ALL  ]                               ^
    [ALL  ] /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.c:66:30: error: 'struct xilinx_vdma_config' has no member named 'stride'
    [ALL  ]    zeddispkit_crtc->dma_config.stride = fb->pitches[0];
    [ALL  ]                               ^
    [ALL  ] /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.c:74:18: error: expected ')' before 'offset'
    [ALL  ]       obj->paddr  offset,
    [ALL  ]                   ^
    [ALL  ] /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.c:73:10: error: too few arguments to function 'dmaengine_prep_slave_single'
    [ALL  ]    desc = dmaengine_prep_slave_single(zeddispkit_crtc->dma,
    [ALL  ]           ^
    [ALL  ] In file included from /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.c:27:0:
    [ALL  ] /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/include/linux/dmaengine.h:710:47: note: declared here
    [ALL  ]  static inline struct dma_async_tx_descriptor *dmaengine_prep_slave_single(
    [ALL  ]                                                ^
    [ALL  ] /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.c: In function 'zeddispkit_drm_crtc_create':
    [ALL  ] /home/adzh/petalinux/components/linux-kernel/xlnx-3.19/drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.c:197:2: error: implicit declaration of function 'drm_crtc_init' [-Werror=implicit-function-declaration]
    [ALL  ]   drm_crtc_init(dev, crtc, &zeddispkit_crtc_funcs);
    [ALL  ]   ^
    [ALL  ] cc1: some warnings being treated as errors
    [ERROR] make[7]: *** [drivers/gpu/drm/zeddispkit/zeddispkit_drm_crtc.o] Error 1
    [ERROR] make[6]: *** [drivers/gpu/drm/zeddispkit] Error 2
    [ERROR] make[5]: *** [drivers/gpu/drm] Error 2
    [ERROR] make[4]: *** [drivers/gpu] Error 2
    [ERROR] make[3]: *** [drivers] Error 2
    [ALL  ] make[3]: *** Waiting for unfinished jobs....
    [ALL  ]   CC      net/ipv4/udplite.o
    [ALL  ]   CC      net/ipv6/udp_offload.o
    [/code]
    ====================================================

    First one has conflict with:

    ====================================================
    [code]
    struct drm_framebuffer *fb = crtc->fb;
    [/code]

    Next three can not find hsize, vsize and stride... (with dma_config defined as xilinx_vdma_config).
    [code]
    zeddispkit_crtc->dma_config.hsize = mode->hdisplay * fb->bits_per_pixel / 8;
    zeddispkit_crtc->dma_config.vsize = mode->vdisplay;
    zeddispkit_crtc->dma_config.stride = fb->pitches[0];
    [/code]
    ====================================================

    All three were previously defined in include/linux/amba/xilinx_dma.h:


    ====================================================
    Kernel 3.6
    [code]
    struct xilinx_vdma_config {
            enum dma_transfer_direction direction;
                                            /* Channel direction */
            int vsize;                      /* Vertical size */
            int hsize;                      /* Horizontal size */
            int stride;                     /* Stride */
            int frm_dly;                    /* Frame delay */
            int gen_lock;                   /* Whether in gen-lock mode */
            int master;                     /* Master that it syncs to */
            int frm_cnt_en;                 /* Enable frame count enable */
            int park;                       /* Whether wants to park */
            int park_frm;                   /* Frame to park on */
            int coalesc;                    /* Interrupt coalescing threshold */
            int delay;                      /* Delay counter */
            int disable_intr;               /* Whether use interrupts */
            int reset;                      /* Reset Channel */
            int ext_fsync;                  /* External Frame Sync */
    };
    [/code]

    Kernel 3.19
    [code]
    struct xilinx_vdma_config {
            int frm_dly;
            int gen_lock;
            int master;
            int frm_cnt_en;
            int park;
            int park_frm;
            int coalesc;
            int delay;
            int reset;
            int ext_fsync;
    };
    [/code]