Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PetaLinux -- Unable to read file uImage
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 364 subscribers
  • Views 1811 views
  • Users 0 members are here
Related

PetaLinux -- Unable to read file uImage

armendzh
armendzh over 10 years ago

I have AVNET Mini-ITX 7z100 board and I been trying to use PetaLinux to build a linux image.

I am, however, unable to boot the uImage... not from the uImage which I created myself from the BSP files for the same board nor from the pre-built BIN and uImage files provided by AVNET.

Here is an error which I am receiving when trying to boot from SDCARD with BOOT.BIN and image.ub:

//=====================================
U-Boot 2015.04 (Apr 06 2016 - 13:45:26)

DRAM:  ECC disabled 1 GiB
MMC:   zynq_sdhci: 0
SF: Detected S25FL128S_64K with page size 512 Bytes, erase size 128 KiB, total 32 MiB
In:    serial
Out:   serial
Err:   serial
Net:   Gem.e000b000
Hit any key to stop autoboot:  0
Device: zynq_sdhci
Manufacturer ID: 3
OEM: 5054
Name: SL64G
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 58.3 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
reading uimage
** Unable to read file uimage **
U-Boot-PetaLinux> run shboot
## Error: "shboot" not defined
U-Boot-PetaLinux> run sdboot
reading uImage
** Unable to read file uImage **
Unknown command '
setenv' - try 'help'
Unknown command 'softdog.nowayout=0' - try 'help'
Wrong Image Format for bootm command
ERROR: can't get kernel image!
//=====================================

Here are commands which I used ot package my BIN and uImage files (I used both and both failed to boot):


//=====================================
petalinux-package --boot --force --format BIN --fsbl images/linux/zynq_fsbl.elf --fpga images/linux/zynq_design_1_wrapper.bit --u-boot --kernel -o image.ub
petalinux-package --boot --force --format BIN --fsbl images/linux/zynq_fsbl.elf --fpga images/linux/zynq_design_1_wrapper.bit --u-boot
//=====================================

I also have another issue of booting the system (both mine and prebuilt) through JTAG. However, I am not sure if both issues are related (booting via JTAG and via SDcard). Here is what I am getting when trying to boot via JTAG:

//=====================================
INFO: Append dtb - /home/adzh/SBIR_MITX/petalinuxProject/MITX_7100_ED/pre-built/linux/images/system.dtb and other options to boot zImage
INFO: Launching XSDB for file download and boot.
INFO: This may take a few minutes, depending on the size of your image.
rlwrap: warning: your $TERM is 'xterm' but rlwrap couldn't find it in the terminfo database. Expect some problems.: Inappropriate ioctl for device
INFO: Configuring the FPGA...                                                                                  
INFO: Downloading bitstream to the target.
                                             
INFO: The XSDB log is as follows
Got $XILINX_SDK: /home/dzhagaryanaa/opt/Xilinx/SDK/2015.2
attempting to launch hw_server

****** Xilinx hw_server v2015.2
  **** Build date : Jun 26 2015-16:42:45
    ** Copyright 1986-1999, 2001-2015 Xilinx, Inc. All Rights Reserved.

INFO: hw_server application started
INFO: Use Ctrl-C to exit hw_server application

INFO: To connect to this hw_server instance use url: TCP:127.0.0.1:3121


Error in startup script:
No supported FPGA device found
    invoked from within
"::tcf::eval -progress ::xsdb::print_progress {::tcf::cache_enter tcfchan#0 {tcf_cache_eval {process_tcf_actions_cache_client ::tcfclient#0::arg}}}"
    (procedure "::tcf::cache_eval_with_progress" line 2)
    invoked from within
"::tcf::cache_eval_with_progress [dict get $arg chan]  [list process_tcf_actions_cache_client $argvar] $progress"
    (procedure "process_tcf_actions" line 1)
    invoked from within
"process_tcf_actions $arg ::xsdb::print_progress"
    (procedure "fpga" line 350)
    invoked from within
"fpga "/home/adzh/SBIR_MITX/petalinuxProject/MITX_7100_ED/pre-built/linux/implementation/download.bit""
//=====================================

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello engsci,

    Are you also using the Mini ITX? Or are you using a diffrent develpoment board/SOM?

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 10 years ago

    Hello engsci,

    Are you also using the Mini ITX? Or are you using a diffrent develpoment board/SOM?

    --Josh