Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Ethernet bidirectional performance
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 539 views
  • Users 0 members are here
Related

Ethernet bidirectional performance

e14 Contributor
e14 Contributor over 9 years ago

Hello!

Has anybody measured the zedboard's ethernet bidirectional performance in linux?

 

I checked the tutorial given in http://zedboard.org/content/updated-open-source-linux-ethernet-performance-test-tutorial-posted but this used iperf3, which, if I'm not mistaken, does not have --dualtest option of iperf2. 

 

I tried using iperf v2 on a custom linux image and I was getting big discrepancies in throughput values. One direction is getting >600Mbps while the other shows <100Mbps. I was wondering if this is hardware related, linux dirver related, or something else.

 

Just a note on my setup, I have a laptop and zedboard directly connected with a Cat5e cable. Ethernet negotiation shows 1000baseT-FD. I need to have the laptop and zedboard communicate simultaneously in realtime, hence the need for bidirectional performance.

 

Thanks!

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello oclabbao,

    I am not aware of any bidirectional ethernet performance tests being done on the Zedboard on our end. You could try asking the same question over at the the Xilinx and Digilent forums in attempt to reach a broader audience.

    https://forum.digilentinc.com/

    https://forums.xilinx.com/

     

    I wouold also caution you with using your RTOS. Please read through this forum post and it discusses some of the challeneges others have faced.

    http://zedboard.org/content/ethernet-throughputperformance

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to jafoste4

    Thanks for the reply Josh. I will try posting at Xilinx and Digilent as you suggexted.

    As for the other forum post (the last link you've given), I've read it before, but these use half-duplex operation if I'm not mistaken. For my own tests, I've no issues with half-duplex. I was able to obtain consistently at least 500Mbps in either direction, and at times even greater than 700 or 800Mbps.

    Thanks again!