Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development SD mounting fails in Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 363 subscribers
  • Views 2034 views
  • Users 0 members are here
Related

SD mounting fails in Linux

e14 Contributor
e14 Contributor over 13 years ago

I've built linux and u-boot according to these references:
http://wiki.xilinx.com/zynq-uboot
http://wiki.xilinx.com/zynq-linux
`
Linux boots, but I cannot access files on the SD card. I can only access the root filesystem from the ramdisk.
`
During boot, I get these messages:
++ Mounting filesystem
mount: mounting /dev/mmcblk0p1 on /mnt failed: No such file or directory
mount: mounting /dev/mmcblk0 on /mnt failed: No such file or directory
`
I don't know where the problem is. Am I missing something in my linux ".config"? Or maybe the device tree source? Or the ramdisk?
`
SD card access is obviously working in ROM/FSBL/u-boot, so it seems like a software issue with linux.
`
Thanks,
David
`
Edit: Maybe other devices aren't working properly either...
<snippet of booting>
Registering SWP/SWPB emulation handler
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
GEM: lp->tx_bd de042000 lp->tx_bd_dma 1e042000 lp->tx_skb ddbfd3c0
GEM: lp->rx_bd de041000 lp->rx_bd_dma 1e041000 lp->rx_skb ddbfd2c0
GEM: MAC 0x00350a00, 0x00002201, 00:0a:35:00:01:22
eth0: no PHY found
XEMACPS mii bus mii_probe fail.
IP-Config: Failed to open eth0
IP-Config: No network devices available
`
Edit2: Seems like I was specifying a fixed ip incorrectly in the device tree, so the ethernet seems happy now, but the MMC is still not working.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi Matthew,
    The mnt directory is there of course, but the mmcblk0 doesn't exist (likewise for mmcblk0 partition 1).

    Seems like the Ethernet problem was unrelated (I think a side effect of me incorrectly modifying the "ip=" of the device tree source, but I have ETH is working now).

    However, I still do not know why the mmcblk0 device is not showing up.

    zynq> ls /dev
    console             network_latency     tty16               tty46
    cpu_dma_latency     network_throughput  tty17               tty47
    device              null                tty18               tty48
    full                psaux               tty19               tty49
    i2c                 ptmx                tty2                tty5
    input               pts                 tty20               tty50
    kmsg                ram0                tty21               tty51
    loop-control        ram1                tty22               tty52
    loop0               ram10               tty23               tty53
    loop1               ram11               tty24               tty54
    loop2               ram12               tty25               tty55
    loop3               ram13               tty26               tty56
    loop4               ram14               tty27               tty57
    loop5               ram15               tty28               tty58
    loop6               ram2                tty29               tty59
    loop7               ram3                tty3                tty6
    mem                 ram4                tty30               tty60
    mice                ram5                tty31               tty61
    mtd0                ram6                tty32               tty62
    mtd0ro              ram7                tty33               tty63
    mtd1                ram8                tty34               tty7
    mtd1ro              ram9                tty35               tty8
    mtd2                random              tty36               tty9
    mtd2ro              root                tty37               ttyPS0
    mtd3                tty                 tty38               urandom
    mtd3ro              tty0                tty39               vcs
    mtd4                tty1                tty4                vcs1
    mtd4ro              tty10               tty40               vcsa
    mtdblock0           tty11               tty41               vcsa1
    mtdblock1           tty12               tty42               xdevcfg
    mtdblock2           tty13               tty43               zero
    mtdblock3           tty14               tty44
    mtdblock4           tty15               tty45
    zynq>

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi Matthew,
    The mnt directory is there of course, but the mmcblk0 doesn't exist (likewise for mmcblk0 partition 1).

    Seems like the Ethernet problem was unrelated (I think a side effect of me incorrectly modifying the "ip=" of the device tree source, but I have ETH is working now).

    However, I still do not know why the mmcblk0 device is not showing up.

    zynq> ls /dev
    console             network_latency     tty16               tty46
    cpu_dma_latency     network_throughput  tty17               tty47
    device              null                tty18               tty48
    full                psaux               tty19               tty49
    i2c                 ptmx                tty2                tty5
    input               pts                 tty20               tty50
    kmsg                ram0                tty21               tty51
    loop-control        ram1                tty22               tty52
    loop0               ram10               tty23               tty53
    loop1               ram11               tty24               tty54
    loop2               ram12               tty25               tty55
    loop3               ram13               tty26               tty56
    loop4               ram14               tty27               tty57
    loop5               ram15               tty28               tty58
    loop6               ram2                tty29               tty59
    loop7               ram3                tty3                tty6
    mem                 ram4                tty30               tty60
    mice                ram5                tty31               tty61
    mtd0                ram6                tty32               tty62
    mtd0ro              ram7                tty33               tty63
    mtd1                ram8                tty34               tty7
    mtd1ro              ram9                tty35               tty8
    mtd2                random              tty36               tty9
    mtd2ro              root                tty37               ttyPS0
    mtd3                tty                 tty38               urandom
    mtd3ro              tty0                tty39               vcs
    mtd4                tty1                tty4                vcs1
    mtd4ro              tty10               tty40               vcsa
    mtdblock0           tty11               tty41               vcsa1
    mtdblock1           tty12               tty42               xdevcfg
    mtdblock2           tty13               tty43               zero
    mtdblock3           tty14               tty44
    mtdblock4           tty15               tty45
    zynq>