Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development SD mounting fails in Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 9 replies
  • Subscribers 363 subscribers
  • Views 2034 views
  • Users 0 members are here
Related

SD mounting fails in Linux

e14 Contributor
e14 Contributor over 13 years ago

I've built linux and u-boot according to these references:
http://wiki.xilinx.com/zynq-uboot
http://wiki.xilinx.com/zynq-linux
`
Linux boots, but I cannot access files on the SD card. I can only access the root filesystem from the ramdisk.
`
During boot, I get these messages:
++ Mounting filesystem
mount: mounting /dev/mmcblk0p1 on /mnt failed: No such file or directory
mount: mounting /dev/mmcblk0 on /mnt failed: No such file or directory
`
I don't know where the problem is. Am I missing something in my linux ".config"? Or maybe the device tree source? Or the ramdisk?
`
SD card access is obviously working in ROM/FSBL/u-boot, so it seems like a software issue with linux.
`
Thanks,
David
`
Edit: Maybe other devices aren't working properly either...
<snippet of booting>
Registering SWP/SWPB emulation handler
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
GEM: lp->tx_bd de042000 lp->tx_bd_dma 1e042000 lp->tx_skb ddbfd3c0
GEM: lp->rx_bd de041000 lp->rx_bd_dma 1e041000 lp->rx_skb ddbfd2c0
GEM: MAC 0x00350a00, 0x00002201, 00:0a:35:00:01:22
eth0: no PHY found
XEMACPS mii bus mii_probe fail.
IP-Config: Failed to open eth0
IP-Config: No network devices available
`
Edit2: Seems like I was specifying a fixed ip incorrectly in the device tree, so the ethernet seems happy now, but the MMC is still not working.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Are you using the kernel from Xilinx or Digilent?  I'm not sure if the Xilinx kernel is compatible with the Zedboard.  Here's the entry for the SD Card from my devicetree, you can check it against yours:

    sdhci@e0100000 {
    tcompatible = "xlnx,ps7-sdhci-1.00.a";
    treg = <0xe0100000 0x1000>;
    tinterrupts = <0x0 0x18 0x0>;
    tinterrupt-parent = <0x1>;
    txlnx,has-cd = <0x1>;
    tclock-frequency = <0x1fc9f08>;
    };

    Matthew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Are you using the kernel from Xilinx or Digilent?  I'm not sure if the Xilinx kernel is compatible with the Zedboard.  Here's the entry for the SD Card from my devicetree, you can check it against yours:

    sdhci@e0100000 {
    tcompatible = "xlnx,ps7-sdhci-1.00.a";
    treg = <0xe0100000 0x1000>;
    tinterrupts = <0x0 0x18 0x0>;
    tinterrupt-parent = <0x1>;
    txlnx,has-cd = <0x1>;
    tclock-frequency = <0x1fc9f08>;
    };

    Matthew