Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Steps to get WLINK8 working using Petalinux on PicoZed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 1265 views
  • Users 0 members are here
Related

Steps to get WLINK8 working using Petalinux on PicoZed

e14 Contributor
e14 Contributor over 10 years ago

First, credit to John Wood who figured out how to get this working on the MicroZed:
http://picozed.org/content/steps-get-wlink-using-petalinux-microzed

I adapted his procedure to work with the PicoZed.

My system:
- PicoZed Rev C02
- PicoZed FMC Carrier Board
- TI WiLink8 WL1837
- Petalinux 2014.4 (kernel 3.17)
- Release 8.6 of the TI drivers

Step 1:  Make a custom cable

Let's get the hard part out of the way.  Make yourself a custom cable to connect the WiLink adapter to the J7 P-mod on the PicoZed carrier board.  For some reason, Avnet changed the pinout on the PicoZed P-mod to be different than that of the MicroZed, so you can't simply plug it in directly.

WiLink adaptor J3  -->   PMOD J7
Pin1                     Pin2
Pin2                     Pin1
Pin3                     Pin8
Pin4                     Pin7
Pin5                     Pin5
Pin6                     Pin6
Pin7                     Pin9
Pin8                     Pin10
Pin9                     Pin3
Pin10                    Pin4
Pin11                    Pin11
Pin12                    Pin12

NOTE: make the cable AS SHORT AS POSSIBLE.  I initially made mine about a finger's length and it proved to be too long to meet the high speed timing requirements of the SDIO interface.

Step 2: Download the TI driver using the build-utilites script.

git://git.ti.com/wilink8-wlan/build-utilites.git

Step 3: Apply patch to kernel

This patch is included in the above build utilites in
build-utilites/patches/kernel_patches/imx-3.14.28/0010-mmc-Add-SDIO-function-devicetree-subnode-parsing.patch 

Note: it will not be applied automatically since the xlnx-3.17 kernel does not have patches associated with it.

Copy the file to the petalinux installation folder:
/opt/PetaLinux/petalinux-v2014.4-final/components/linux-kernel/xlnx-3.17
cd into that folder and type:
patch -p1 < 0010-mmc-Add-SDIO-function-devicetree-subnode-parsing.patch

Step 4: Enable the necessary settings. 

In the build-utilites folder you got from git take a look at the 'base_config=' section.  These settings need to be enabled.  I was able to find all but one setting in the petalinux configuration this was CONFIG_
WIRELESS_EXT. In petalinux this appears to be private. To make this visible I modified the Kconfig in /opt/PetaLinux/petalinux-2014.4-final/components/linux-kernel/xlnx-3.17/net/wireless/ as shown:
config WIRELESS_EXT
bool "Enable Wireless Extensions"
default n

Then run petalinux-config -c kernel, each line shows the text menu items:
Cryptographic API -->
tu2022 CCM Support
tu2022 GCM Support
tu2022 EC8 Support
tu2022 Michael Mic keyed digest algorithm
tu2022 Arc4 cipher algorithm
Library Functions -->
tu2022 CRC 7 Functions
Device Drivers -->
tu2022 Input Device Support
tu2022 Misc...Devices
tu2022 User Level Driver Support
Networking -->
tu2022 RF Switch subsystem support
Security Options -->
tu2022 Enable Access Key Retention Support
tu2022 Enable Different Security Modules


These should be all the kernel config changes you need to make.

Step 5: Build Petalinux with these settings
type 'petalinux-build' from the command line in your project directory

Step 6: Modify setup-env

I took John's advice and created a petalinux app that will copy the fs directory to the TARGET ROOT, which allows you to make updates to the configuration without wiping out files I put directly into target root. My setup-env is shown below. I will cover the app for copying later.
                             //
#                           -(o o)-
#========================oOO==(_)==OOo=======================
# This file contains the exports needed for automating the
# build process of WLAN components.
# Place this file in the same directory with wl18xx_build.sh
# build scripts. No need to run 'source setup-env', the build
# scripts will perform it internally.
#===========================================================
# User specific environment settings - use full PATH
# if DEFAULT toolchain path is set toolchain will be downloaded to ./toolchain.
export TOOLCHAIN_PATH=/opt/PetaLinux/petalinux-v2014.4-final/tools/linux-i386/arm-xilinx-linux-gnueabi/bin
# if DEFAULT path to root filesystem is set ./fs folder will be used.
export ROOTFS=~/Embedded/wlink_test/software/wlink/components/apps/wireless/fs/components/apps/wireless/fs
#export ROOTFS=DEFAULT
#if DEFAULT kernel path is set - kernel will be downloaded (set branch to match kernel version)
export KERNEL_PATH=~/Embedded/wlink_test/software/wlink/build/linux/kernel/xlnx-3.17
# if KERNEL_VARIANT below is set the build script will look for kernel specific
# patches under the patches directory:
# - patches under the patches/driver_patches/$KERNEL_VARIANT directory would be
# applied during "modules" build.
# - patches under the patches/kernel_patches/$/$KERNEL_VARIANT directory would
# be applied to the kernel pointed by KERNEL_PATH in case the "patch_kernel"
# command is used.
# Note: the kernel is not built automatically after the patches are applied
export KERNEL_VARIANT=xlnx-3.17
export CROSS_COMPILE=arm-xilinx-linux-gnueabi-
export ARCH=arm
[ "$TOOLCHAIN_PATH" != "DEFAULT" ] && export PATH=$TOOLCHAIN_PATH:$PATH

Step 7: Create Petalinux App

a. I created a petalinux app called wireless, deleted the C file, and modified the make file as shown
b. create fs subdriectory for copying files in
ifndef PETALINUX
$(error "Error: PETALINUX environment variable not set. Change to the root of your PetaLinux install, and source the settings.sh file")
endif
include apps.common.mk
APP = settings

all: build install

.PHONY: build
build:
install:
t# Copy settings files to the rootfs.
tcp -r ./fs/* $(TARGETDIR)
clean:

Step 8: Add startup of modules to /etc/modules in /wireless/fs directory

# /etc/modules: kernel modules to load at boot time.
#
# This file contains the names of kernel modules that should be loaded
# at boot time, one per line. Lines beginning with "#" are ignored.
# Parameters can be specified after the module name.
wlcore_sdio
Wl18xx

Step 9: Add wl18xx-conf.bin to fs directory in the project you made

You need to generate this using the configureation.sh script in build-utilites
Then copy the file to:
/fs/lib/firmware/ti-connectivity/wl18xx-conf.bin

Step 10: Run the build script using update R8.6

./sudo_build_wl18xx.sh update R8.6

Step 11: Fix issue with Precistion Timing GPIO

When going to 8.6 there is a new requirement for a GPIO which is not on the picozed for a precision timing output. This will preclude the driver from loading. Comment out the request for this line in the following file.
src/driver//drivers/net/wireless/ti/wlcore/main.c (approx line 6450)
#if 0 <--- do this
/* time sync */
wl->time_sync.gpio = 66;
ret = gpio_request_one(wl->time_sync.gpio, GPIOF_DIR_OUT, "time_sync");
if (ret < 0) {
wl1271_error("error requesting time_sync gpio");
goto err_buffer_32;
}
wl1271_info("Time Sync: gpio requested");
#endif <--- and this

Step 12: Rebuild the TI drivers

Do not use update or your change will be lost.
./sudo_build_wl18xx.sh

Step 13: Update device tree.
Assuming you are using the petalinux structure for a picozed, you should only need to change which SDIO you are using and which gpio pin is used for enable and which is used for the interrupt for a custom board...
/dts-v1/;
/include/ "system-conf.dtsi"
/ {
twlan_en: fixedregulator@2 {
tcompatible = "regulator-fixed";
tregulator-name = "wlan-en-regulator";
tregulator-min-microvolt = <0x325aa0>;
tregulator-max-microvolt = <0x325aa0>;
tgpio = <&gpio0 0x9 0x4>; <<<<<<<<< gpio 9
tstartup-delay-us = <0x11170>;
tenable-active-high;
t};
};

&gem0 {
tphy-handle = <&phy0>;
tphy-mode = "rgmii-id";
tmdio {
tt#address-cells = <1>;
tt#size-cells = <0>;
ttphy0: phy@0 {
tttcompatible = "marvell,88e1510";
tttdevice_type = "ethernet-phy";
tttreg = <0x0>;
tttmarvell,reg-init = <3 16 0xff00 0x1e 3 17 0xfff0 0x00>;
tt};
t};
};

&qspi {
tflash0: flash@0 {
tcompatible = "micron,n25q128a13";
t};
};

&gpio0 { <<<<< make gpio an int controller for gpio ints
tinterrupt-controller;
t#interrupt-cells = <2>;
};

&sdhci1{ <<<<<<< SDIO 1
tvmmc-supply = <&wlan_en>;
tbus-width = <4>;
tti,non-removable;
tti,needs-special-hs-handling;
tcap-power-off-card;
tkeep-power-in-suspend;
t#address-cells = <1>;
t#size-cells = <0>;
twlcore: wlcore@0 {
ttcompatible = "ti,wl1837";
ttinterrupt-parent = <&gpio0>;
ttinterrupts = <0 4>; <<<<<<GPIO pin 0, note GPIO is used as int parent
ttreg = <2>;
ttplatform-quirks = <0x1>;
ttboard-ref-clock = <0x4>;
t};
};

Step 13: Image will be too big

You need to increase the mem offset in two places:
1. petalinux-config --> uboot configuration - netboot offset change from hex 0x1000000 to desired value - my image.ub ~20M, but I set it to 0x3000000.
2. In your ./subsystems/linux/configs/u-boot/platform-top.h change CONFIG_SYS_BOOTM_LEN from 0x1000000 to same value 0x3000000.
u00A0
*** Must rebuild the whole project in order for this to take effect (includes new BOOT.bin and image.ub)  ***

You should now be able to see the wlan0 interface when you boot up and type ifconfig -a

Below are some of the messages displayed during boot that indicate a correct initialization of the WiLink module:
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-arasan e0101000.sdhci: No vqmmc regulator found
mmc1: SDHCI controller on e0101000.sdhci [e0101000.sdhci] using ADMA
sdhci-arasan e0101000.sdhci: card claims to support voltages below defined range
mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
mmc1: new high speed SDIO card at address 0001
Loading modules backported from Linux version R8.6-0-g3f5b34f
Backport generated by backports.git ol_r8.a9.28-0-g4677dc3
cfg80211: Calling CRDA to update world regulatory domain
wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
wlcore: loaded
wlcore: driver version: R8.6-dirty
wlcore: compilation time: Tue Jan 19 16:03:08 2016
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: Calling CRDA to update world regulatory domain
cfg80211: Exceeded CRDA call max attempts. Not calling CRDA

The CRDA timeout I haven't figured out yet, but the wlan0 interface is detected and can connect to wireless networks successfully.  The timeout, from what I've read, may have something to do with busybox mdev not detecting a kernel event.


  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Thanks for sharing this Brett!

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    hi..

    when run ./sudo_build_wl18xx.sh update R8.6

    y original source files ...
    Applying patches from patches to /home/jkpark/wilink/build-utilites/src/compat_wireless ...
    Modify Kconfig tree ...
    Rewrite Makefiles and Kconfig files ...
    Done!
    Generating local configuration database from kernel ... done.
    cc -Wall -Wmissing-prototypes -Wstrict-prototypes -O2 -fomit-frame-pointer -c -o conf.o conf.c
    as: unrecognized option '--64'
    make[2]: *** [conf.o] Error 1
    make[1]: *** [defconfig-wl18xx] Error 2
    make: *** [defconfig-wl18xx] Error 2
    /--------------
    | Your backport package isn't configured, please configure it
    | using one of the following options:
    | To configure manually:
    | make oldconfig
    | make menuconfig
    |
    | To get defaults for certain drivers:
    | make defconfig-alx
    | make defconfig-ar5523
    | make defconfig-ath10k
    | make defconfig-ath5k
    | make defconfig-ath6kl
    | make defconfig-ath9k
    | make defconfig-ath9k-debug
    | make defconfig-b43
    | make defconfig-b43legacy
    | make defconfig-brcmfmac
    | make defconfig-brcmsmac
    | make defconfig-carl9170
    | make defconfig-cw1200
    | make defconfig-hwsim
    | make defconfig-igb
    | make defconfig-iwlwifi
    | make defconfig-nfc
    | make defconfig-rtlwifi
    | make defconfig-wcn36xx
    | make defconfig-wifi
    | make defconfig-wil6210
    | make defconfig-wl18xx
    | make defconfig-wwan
    make[2]: *** [.config] Error 1
    make[1]: *** [modules] Error 2
    make: *** [default] Error 2
    ****** ERROR 0 *******

    setup-env
    # //
    # -(o o)-
    #========================oOO==(_)==OOo=======================
    # This file contains the exports needed for automating the
    # build process of WLAN components.
    # Place this file in the same directory with wl18xx_build.sh
    # build scripts. No need to run 'source setup-env', the build
    # scripts will perfom it internaly.
    #===========================================================
    # User specific environment settings - use full PATH

    # if DEFAULT toolchain path is set toolchain will be downloaded to ./toolchain.
    export TOOLCHAIN_PATH=/opt/Xilinx/SDK/2015.4/gnu/arm/lin/arm-xilinx-linux-gnueabi/bin

    # if DEFAULT path to root filesystem is set ./fs folder will be used.
    export ROOTFS=/home/jkpark/petalinux20144/test/fs

    #if DEFAULT kernel path is set - kernel will be downloaded (set branch to match kernel version)
    export KERNEL_PATH=/home/jkpark/petalinux20144/test/build/linux/kernel/xlnx-3.17
    #export KERNEL_PATH=/home/jkpark/temp/wl18xx

    # if KERNEL_VARIANT below is set the build script will look for kernel specific
    # patches under the patches directory:
    # - patches under the pathces/driver_patches/$KERNEL_VARIANT directory would be
    # applied during "modules" build.
    # - patches under the patches/kernel_patches/$/$KERNEL_VARIANT directory would
    # be applied to the kernel pointed by KERNEL_PATH in case the "patch_kernel"
    # command is used.
    # Note: the kernel is not built automatically after the patches are applied
    export KERNEL_VARIANT=xlnx-3.17

    export CROSS_COMPILE=arm-xilinx-linux-gnueabi-
    export ARCH=arm
    [ "$TOOLCHAIN_PATH" != "DEFAULT" ] && export PATH=$TOOLCHAIN_PATH:$PATH

    how can solve this problem ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I can't help you much here other than noticing that your TOOLCHAIN_PATH in setup-env indicates you are using Xilinx SDK 2015.4.  I developed using SDK 2014.4 and can only verify that it works on this version.  I highly recommend that you don't mix versions (2015.4 SDK toolchain and Petalinux 2014.4) since they will most likely not play nicely together.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Update:  I've recently upgraded my Petalinux to 2015.4 and needed to rebuild the Wilink drivers to work with it.  The latest drivers work better as I didn't have to apply so many patches and debug any source code to get them to work.  Below are the steps I took to get it working.

     

    My system:
    - PicoZed Rev C02
    - Custom carrier board (don't have to make that stupid custom PMOD cable this time!)
    - TI WiLink8 WL1837
    - Petalinux 2015.4 (xlnx-4.0 kernel)
    - Release 8.7_SP1 of the TI drivers

     

    Step 1: Download the TI driver using the build utilties script.

    On your Linux host, cd into some folder and type:

    git clone git://git.ti.com/wilink8-wlan/build-utilites.git

    then

    ./build_wl18xx.sh init

     

    Step 2: Reconfigure the kernel

    Enable the necessary settings.  I was able to find all but one setting in the petalinux configuration this was CONFIG_

    WIRELESS_EXT. In petalinux this appears to be private. To make this visible I modified the Kconfig in /opt/PetaLinux/petalinux-2015.4-final/components/linux-kernel/xlnx-4.0/net/wireless/ as shown:

    config WIRELESS_EXT

    bool "Enable Wireless Extentions"

    default n

     

    Then run petalinux-config -c kernel, each line shows the text menu items:

    Cryptographic API -->

    •   CCM Support
    •   GCM Support
    •   EC8 Support
    •   Michael Mic keyed digest algorithm
    •   Arc4 cipher algorithm

    Library Functions -->

    •   CRC 7 Functions

    Device Drivers -->

    •   Input Device Support
    •   Misc...Devices
    •   User Level Driver Support

    Networking -->

    •   RF Switch subsystem support

    Security Options -->

    •   Enable Access Key Retention Support
    •   Enable Different Security Modules

     

    NOTE: Do NOT enable CONFIG_NETFILTER.  This conflicts with the compat.ko module in the TI Wilink driver.

     

    Step 3: Build Petalinux with these settings

    petalinux-build

     

    Step 4: Modify setup-env

    In this case I have created a petalinux app that will copy the fs directory to the TARGET ROOT, this allows me to make updates to the configuration without wiping out files I put directly into target root. My setup-env is shown below. I will cover the app for copying later.

                                 \\\//

    #                           -(o o)-

    #========================oOO==(_)==OOo=======================

    # This file contains the exports needed for automating the

    # build process of WLAN components.

    # Place this file in the same directory with wl18xx_build.sh

    # build scripts. No need to run 'source setup-env', the build

    # scripts will perform it internally.

    #===========================================================

    # User specific environment settings - use full PATH

     

    # if DEFAULT toolchain path is set toolchain will be downloaded to ./toolchain.

    export TOOLCHAIN_PATH=/opt/PetaLinux/petalinux-v2015.4-final/tools/linux-i386/arm-xilinx-linux-gnueabi/bin

     

    # if DEFAULT path to root filesystem is set ./fs folder will be used.

    export ROOTFS=~/Documents/Project/components/apps/wifi/targetroot

     

    #if DEFAULT kernel path is set - kernel will be downloaded (set branch to match kernel version)

    export KERNEL_PATH=~/Documents/Project/build/linux/kernel/xlnx-4.0

     

    # if KERNEL_VARIANT below is set the build script will look for kernel specific

    # patches under the patches directory:

    # - patches under the pathces/driver_patches/$KERNEL_VARIANT directory would be

    #   applied during "modules" build.

    # - patches under the patches/kernel_patches/$/$KERNEL_VARIANT directory would

    #   be applied to the kernel pointed by KERNEL_PATH in case the "patch_kernel"

    #   command is used.

    #   Note: the kernel is not built automatically after the patches are applied

    export KERNEL_VARIANT=xlnx-4.0

     

    export CROSS_COMPILE=arm-xilinx-linux-gnueabi-

    export ARCH=arm

    [ "$TOOLCHAIN_PATH" != "DEFAULT" ] && export PATH=$TOOLCHAIN_PATH:$PATH

     

    Step 5: Create Petalinux App

    a. I created a petalinux app called wifi, deleted the C file, and modified the makefile as shown

    b. create targetroot subdirectory for copying files in

    ifndef PETALINUX

    $(error "Error: PETALINUX environment variable not set. Change to the root of your PetaLinux install, and source the settings.sh file")

    endif

    include apps.common.mk

    APP = settings

     

    all: build install

     

    .PHONY: build

    build:

    install:

    # Copy settings files to the rootfs.

    cp -r ./targetroot/* $(TARGETDIR)

    clean:

     

    Step 6. Run the build script using update R8.7_SP1

    Then take all the modules.* files in targetroot/lib/modules/4.0.0-xilinx and put them into their own folder there (e.g. wilink_mods) so they don't overwrite the modules files PetaLinux creates.

     

    Step 7. Update device tree.

    All the info I found was for flat trees, this is the latest format assuming using the petalinux structure for a picozed, you should only need to change which SDIO you are using and which gpio pin is used for enable and which is used for the interrupt for a custom board...

    /dts-v1/;

    /include/ "system-conf.dtsi"

    / {

    wlan_en: fixedregulator@2 {

    compatible = "regulator-fixed";

    regulator-name = "wlan-en-regulator";

    regulator-min-microvolt = <0x325aa0>;

    regulator-max-microvolt = <0x325aa0>;

    gpio = <&gpio0 0x9 0x4>; <<<<<<<<< gpio 9

    startup-delay-us = <0x11170>;

    enable-active-high;

    };

    };

     

    &gem0 {

    phy-handle = <&phy0>;

    phy-mode = "rgmii-id";

    mdio {

    #address-cells = <1>;

    #size-cells = <0>;

    phy0: phy@0 {

    compatible = "marvell,88e1510";

    device_type = "ethernet-phy";

    reg = <0x0>;

    marvell,reg-init = <3 16 0xff00 0x1e 3 17 0xfff0 0x00>;

    };

    };

    };

     

    &qspi {

    flash0: flash@0 {

    compatible = "micron,n25q128a13";

    };

    };

     

    &gpio0 { <<<<< make gpio an int controller for gpio ints

    interrupt-controller;

    #interrupt-cells = <2>;

    };

     

    &sdhci1{ <<<<<<< SDIO 1

    vmmc-supply = <&wlan_en>;

    bus-width = <4>;

    ti,non-removable;

    ti,needs-special-hs-handling;

    cap-power-off-card;

    keep-power-in-suspend;

    #address-cells = <1>;

    #size-cells = <0>;

    wlcore: wlcore@0 {

    compatible = "ti,wl1837";

    interrupt-parent = <&gpio0>;

    interrupts = <50 4>; <<<<<<GPIO pin 50, note GPIO is used as int parent

    reg = <2>;

    platform-quirks = <0x1>;

    board-ref-clock = <0x4>;

    };

    };

     

    Step 8: Image will be too big

    You need to increase the mem offset in two places:

    1. petalinux-config --> uboot configuration - netboot offset change from hex 0x1000000 to desired value - my image.ub ~20M, but I set it to 0x2000000 (32MB).

    2. In your ./subsystems/linux/configs/u-boot/platform-top.h change CONFIG_SYS_BOOTM_LEN from 0x1000000 to same value 0x2000000.

     

    Step 9:  Create a startup script that will run at boot time (see petalinux reference tools doc) and insert the modules in this order:

    insmod /lib/modules/4.0.0-xilinx/updates/compat/compat.ko

    insmod /lib/modules/4.0.0-xilinx/updates/net/wireless/cfg80211.ko

    insmod /lib/modules/4.0.0-xilinx/updates/net/mac80211/mac80211.ko

    insmod /lib/modules/4.0.0-xilinx/updates/drivers/net/wireless/ti/wlcore/wlcore.ko

    insmod /lib/modules/4.0.0-xilinx/updates/drivers/net/wireless/ti/wlcore/wlcore_sdio.ko

    insmod /lib/modules/4.0.0-xilinx/updates/drivers/net/wireless/ti/wl18xx/wl18xx.ko

     

    Step 10: Rebuild the entire petalinux-project

    •   petalinux-build (to get image.ub)
    •   petalinux-package --boot --fsbl <FSBL image> --fpga <FPGA bitstream> --u-boot (to generate BOOT.bin)

     

    Step 11: Boot the board with the built images.

     

    Step 12:  Configure the Wilink chip.

    Generate the wl18xx-conf.bin by running /usr/sbin/wlconf/configure-device.sh)

    Copy to /targetroot/lib/firmware/ti-connectivity/wl18xx-conf.bin in the Petalinux wifiapp you created.  Then run petalinux-build again.  This is the final image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    For anyone coming across this post, the TI drivers for the WILINK8 have been mainlined starting with Linux kernel 4.1.  No more out of tree builds!  Simply enable the drivers in the kernel configuration and the rest should take care of itself.