Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Dynamically Configure FPGA From Host Program
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 352 views
  • Users 0 members are here
Related

Dynamically Configure FPGA From Host Program

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I was wondering if anyone knows an efficient way to program the FPGA(PL) from a host C program (not on the SoC, but from the host PC). Is there an Xilinx API I can use/include in my program. As the only way I can think of doing it at the moment is invoking command line programming via Impact.

Basically I want to put the SDK "Program FPGA" functionality in my host C program where the user selects a prebuilt .bit file (and elf file if possible) to program the FPGA/SoC. This is just for a test of concept, later I would like to put this dynamic configuration onto on of the ARM CPU's.

Many Thanks
Sam

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    You might want to take a look at this Xilinx design example:

     

    http://www.xilinx.com/support/answers/46913.htm

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    And why would that help him?
    (Actually he wrote: "(not on the SoC, but from the _host PC_)".)

    Unfortunately the Xilinx JTAG API is not public. The easiest way is to call impact from your software.

    Or - if you are determined - you can use the Digilent API to access the JTAG cable functions. And then you create an svf file from the programming bitfil, and with that you can program the FPGA from the host PC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    And why would that help him?
    (Actually he wrote: "(not on the SoC, but from the _host PC_)".)

    Unfortunately the Xilinx JTAG API is not public. The easiest way is to call impact from your software.

    Or - if you are determined - you can use the Digilent API to access the JTAG cable functions. And then you create an svf file from the programming bitfil, and with that you can program the FPGA from the host PC.