Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Only first access to GPIO seems to work.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 495 views
  • Users 0 members are here
Related

Only first access to GPIO seems to work.

e14 Contributor
e14 Contributor over 8 years ago

Hi,


When I access GPIO from C code, only the first access goes through. Further access are basically ignored. I need to close the value file and reopen to do another access. 

Everything works fine I I echo value from shell, thou
gh. So I'm not sure what is the problem ?

 

Below is the working C code after modyfing it to close and reopen after every access:


#include <stdio.h>
 
int main()
{
 FILE *gp;
    int i;
    printf("Open file\n");
    gp = fopen("/sys/class/gpio/gpio939/value", "w");
    for ( i =0; i < 10; i++) {
       fputs("0", gp);
fclose(gp);
gp = fopen("/sys/class/gpio/gpio939/value", "w");
       fputs("1", gp);
fclose(gp);
gp = fopen("/sys/class/gpio/gpio939/value", "w");
    }
    printf("Close File\n");
    fclose(gp);
    printf("Done\n");
    return 0;
}
  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 8 years ago

    I'm not sure exactly what the problem is, but check out these links to see if there is anything helpful.

    https://forums.xilinx.com/t5/General-Technical-Discussion/Accessing-AXI-GPIO-using-UIO-drivers-in-Linux/td-p/520479
    https://forums.xilinx.com/t5/Embedded-Linux/AXI-GPIO-Support/td-p/240988


    Check out using UIO.
    http://www.wiki.xilinx.com/Zynq-7000+AP+SoC+Spectrum+Analyzer+part+5+-+Accelerating+Software+-+Accelerating+an+FFT+with+ACP+Coprocessor+Tech+Tip+2014.3 

    http://fpga.org/2013/05/28/how-to-design-and-access-a-memory-mapped-device-part-one/

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    ok seems this behavior is expected, according to info provided at: https://falsinsoft.blogspot.ca/2012/11/access-gpio-from-linux-user-space.html