Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Configure PL from PS
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 782 views
  • Users 0 members are here
Related

Configure PL from PS

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I try to configure the PL from PS. Therefor I use the xdevcfg_polled_example.c from the xdevcfg documentation (just clicking in the .mss file).
The problem is, that it always hangs when polling the done flag in line 280.
I have no ide why.
I have used the .bin file from Vivado output and one generated by promgen (they are slightly different), but both did not work.
When first configurating the FPGA with JTAG and then reconfigurating with the example program, it does not hang and the logic is configured the right way. But that actually is not what I'm tryin to achieve.
Interestingly I found out, that when letting the debugger run free in that loop for some time, a reset occurs (just as if a buffer overflow occurs).


Can somebody help?


Best regards,
Yaro

P.S. I use Vivado 2014.2

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    There are a couple of posts on the Xilinx Community forum that might be helpful:

     

    http://forums.xilinx.com/t5/Zynq-All-Programmable-SoC/Full-PL-configuration-using-PCAP/m-p/392335/highlight/true#M828

     

    http://forums.xilinx.com/t5/Embedded-Processor-System-Design/Zynq-PL-configuration-interfaces/m-p/317951/highlight/true#M8070

     

    As the second one suggests you might want to look at XAPP1159.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    There are a couple of posts on the Xilinx Community forum that might be helpful:

     

    http://forums.xilinx.com/t5/Zynq-All-Programmable-SoC/Full-PL-configuration-using-PCAP/m-p/392335/highlight/true#M828

     

    http://forums.xilinx.com/t5/Embedded-Processor-System-Design/Zynq-PL-configuration-interfaces/m-p/317951/highlight/true#M8070

     

    As the second one suggests you might want to look at XAPP1159.

     

    -Gary