Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zedboard - Problem using GPIO in Linux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 363 subscribers
  • Views 854 views
  • Users 0 members are here
Related

Zedboard - Problem using GPIO in Linux

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I have a problem using an GPIO interface in my self compilied linux. I followed all steps of Session 11 of Mohammadsadegh Sadri (https://www.youtube.com/user/mamsadegh2/videos), and the related entries in the Xilinx Wiki (http://www.wiki.xilinx.com/). I managed to compile Linux, u-boot and all nessesarie stuff. I have BOOT.ini on my SD-Card which contains the FSBL, the bitstream file and the uboot. The system boots fine and uboot loads the ramdisk, uImage and deviceTree file using FTFP from my workstation. The system boots fine and I can access the linux using the UART interface.

The hardware design I'm using contains the Zynq core and two additional GPIO ports, one connected to the 8 LED's on the board and the other connected to the push buttons.

In Linux I see 3 different GPIO devices under /sys/classes/gpio/. When I follow the istructions in the Wiki about GPIO the export of the GPIO devices works properly. But when I try to set the GPIO direction of the GPIO device to "out" the system crashes without any error message.

How could I trace the Problem? Any tips of solving the issus?

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    I know that the numbering changed recently. Take a look at the PicoZed FMC Carrier Getting Started Guide v2.0, which was based on PetaLinux 2014.4.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    Hi Bryan Fletcher ,I am also facing the same problem. But I am using Zedboard (Not PicoZed) and running petalinux 2015v1.2.

    The valid GPIO's that i can export are between 885 to 1023. 

    I can set the direction for GPIO's between 906-1023. But when i try to change the direction of GPIO's between 885-905 the system crashes.

    What may be the issue.

    Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hello Darshan,

     

    It looks like the GPIO offset has changed in PetaLinux 2015.2. The range is now 906 to 1023, as your results indicate.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Gary Edwards,

    Yes it might have changed. But I am not able to set the direction of gpio's between 885-905. The system crashes if i try to set and the zedboard should be restarted.

    What might be the issue.

    Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    As the lowest GPIO range is now 906, writing to an address below that is probably conflicting with memory associated with some other function used in your system, which will produce unpredictable results.

     

    -Gary