Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development RAMDISK does not Work on ZedBoard
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 685 views
  • Users 0 members are here
Related

RAMDISK does not Work on ZedBoard

e14 Contributor
e14 Contributor over 11 years ago

Hi

I try to get the lates Digilent-Linux to run on a Zedboard:
Linux version 3.12.0-xilinx-dirty (build@build-skywalker) (gcc version 4.7.4 (Ubuntu/Linaro 4.7.4-2ubuntu1) )

I run into trouble using the initrd as ramdisk.
On the ZedBoard I get the
RAMDISK: Couldn't find valid RAM disk image starting at 0.
error.
Which tells me nothing. And I am now googling all day :(

The same zImage, device.dtb, ramdisk.gz runs find on qemu (Xilinx GIT).

I have to add, I start linux from SD card directly from FSBL.
My chosen-part of the dts contains this:
linux,initrd-start = 0x800000;
linux,initrd-end = 0x8510000;

Linux is loaded at 0x02000000, DTD at 0x01000000.

I see, initrd RAM is freed:
Freeing initrd memory: 324K (c0800000 - c0851000)

Any hint what I can do ...

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    Hopefully some other user can help you as we do not use Digilent-Linux here at Avnet. You may have better luck contacting Digilent directly.

    support@digilentinc.com

    https://www.digilentinc.com/Support/Support.cfm

     

    If you are willing to consider an alternative to the Digilent-Linux, you may try Silica's Yocto project for ZedBoard:

    https://www.yoctoproject.org/organization/silica

    http://architechboards-zedboard.readthedocs.org/en/latest/index.html

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    and get the next Linux source tree :-) I also have the Xilinx tree. But this one doesn't boot at all.
    BTW: Since it is Avnet/Digilent stamped on the board, I thought the "official" Zedboard.org version is the Digilent one.

    Cheers,
    42Bastian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago

    ZedBoard is used for both commercial development and for education. If you are a student, then the Digilent distribution may be the official one. Digilent provides the support to education-related users.

     

    Are you also having trouble with the Xilinx distribution? I'm not aware of any issues with that currently.

     

    Bryan