Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development many bit file into PL
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 271 views
  • Users 0 members are here
Related

many bit file into PL

100gma
100gma over 12 years ago

hello,

1/ i have zedBoard, and i need to load different bit file, can i load more then one bit file or i must include the add design into only bit file

2/ the bit file, will be placed inti PL ?


thank you

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    When you generate the new bitstream, you can then export the current hardware which overwrites the bit file that you had previously. Your sdk should then give you an option so that the hardware platfrom and bsp change automatically with your new hardware that you exported.

    In your second question, are you asking if the bit file is what is used to program the FPGA in the PL? If so, the answer is yes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100gma
    0 100gma over 12 years ago

    hello,

    first let me thank you for your response,

    i have a bit file, but it's generated by XPS ( xilinx tools ), the problem that i need to add a new bloc design to this architecture with vivado, then i will get another bit file, so it's possible de load 2 bit file, or when i will generate the boot.ini file, i will add those 2 bit file, and then copy all bootable file ( include the 2 bit file ) to SD card ?

    thank you for the second response ;)

    have a nice day