Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Zedboard AMP solution
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 363 subscribers
  • Views 550 views
  • Users 0 members are here
Related

Zedboard AMP solution

e14 Contributor
e14 Contributor over 13 years ago

Hello all,

I am trying out the Pre-canned AMP solution ( baremetal + Linux) on my Zedboard and i am facing some issues in getting it to work.

Initially i used the zynq-beta tagged repository to build by uboot from source and i could not make it work.
After that i also tried the xilinx-v14.5 tagged repository as mentioned in the Read me for the design Tutorial but still i get the same error

The error is i am not able to mount my ramdisk. The kernel Log is as below





Booting Linux on physical CPU 0x0
Linux version 3.8.0-xilinx (rs71ein@einz1693) (gcc version 4.7.2 (GCC) ) #1 SMP PREEMPT Mon Aug 5 19:37:27 CEST 2013
CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine: Xilinx Zynq Platform, model: ZedBoard
bootconsole [earlycon0] enabled
INITRD: 0x1f8ca000+0x0028ac63 is not a memory region - disabling initrd
cma: CMA: reserved 16 MiB at 16c00000
Memory policy: ECC disabled, Data cache writealloc
PERCPU: Embedded 7 pages/cpu @c08c1000 s7616 r8192 d12864 u32768
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 97536
Kernel command line: console=ttyPS0,115200 root=/dev/ram maxcpus=1 rw ip=110.0.0.5::110.0.0.1:255.255.255.0::eth0:dhcp earlyprintk
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
__ex_table already sorted, skipping sort
Memory: 384MB = 384MB total
Memory: 367332k/367332k available, 25884k reserved, 0K highmem
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)
    vmalloc : 0xd8800000 - 0xff000000   ( 616 MB)
    lowmem  : 0xc0000000 - 0xd8000000   ( 384 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .text : 0xc0008000 - 0xc052a754   (5258 kB)
      .init : 0xc052b000 - 0xc0554dc0   ( 168 kB)
      .data : 0xc0556000 - 0xc058e9e8   ( 227 kB)
       .bss : 0xc058e9e8 - 0xc05b8f98   ( 170 kB)
Preemptible hierarchical RCU implementation.
        Dump stacks of tasks blocking RCU-preempt GP.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
NR_IRQS:16 nr_irqs:16 16
xslcr mapped to d8802000
Zynq clock init
ps7-ttc #0 at d8804000, irq=43
sched_clock: 32 bits at 100 Hz, resolution 10000000ns, wraps every 4294967286ms
Console: colour dummy device 80x30
Calibrating delay loop... 1064.96 BogoMIPS (lpj=5324800)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x3b7910 - 0x3b7944
L310 cache controller enabled
l2x0: 8 ways, CACHE_ID 0x000000c0, AUX_CTRL 0x72360000, Cache size: 524288 B
Brought up 1 CPUs
SMP: Total of 1 processors activated (1064.96 BogoMIPS).
devtmpfs: initialized
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
xgpiops e000a000.ps7-gpio: gpio at 0xe000a000 mapped to 0xd880c000
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
Switching to clocksource xttcps_clocksource
NET: Registered protocol family 2
TCP established hash table entries: 4096 (order: 3, 32768 bytes)
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)
TCP: Hash tables configured (established 4096 bind 4096)
TCP: reno registered
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
hw perfevents: enabled with ARMv7 Cortex-A9 PMU driver, 7 counters available
jffs2: version 2.2. (NAND) (SUMMARY)  u00A9 2001-2006 Red Hat, Inc.
msgmni has been set to 749
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
dma-pl330 f8003000.ps7-dma: Loaded driver for PL330 DMAC-267056
dma-pl330 f8003000.ps7-dma:     DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
e00010console [ttyPS0] enabled, bootconsole disabled
console [ttyPS0] enabled, bootconsole disabled
xdevcfg f8007000.ps7-dev-cfg: ioremap f8007000 to d8862000 with size 1000
brd: module loaded
loop: module loaded
xspips e0006000.ps7-spi: master is unqueued, this is deprecated
xspips e0006000.ps7-spi: at 0xE0006000 mapped to 0xD8864000, irq=58
xspips e0007000.ps7-spi: master is unqueued, this is deprecated
xspips e0007000.ps7-spi: at 0xE0007000 mapped to 0xD8866000, irq=81
xqspips e000d000.ps7-qspi: master is unqueued, this is deprecated
m25p80 spi2.0: found s25fl256s1, expected n25q128
m25p80 spi2.0: fallback to 3-byte address mode
m25p80 spi2.0: maximum accessible size is 16MB
m25p80 spi2.0: s25fl256s1 (32768 Kbytes)
5 ofpart partitions found on MTD device spi2.0
Creating 5 MTD partitions on "spi2.0":
0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
0x000000100000-0x000000600000 : "qspi-linux"
0x000000600000-0x000000620000 : "qspi-device-tree"
0x000000620000-0x000000c00000 : "qspi-rootfs"
0x000000c00000-0x000001000000 : "qspi-bitstream"
xqspips e000d000.ps7-qspi: at 0xE000D000 mapped to 0xD8868000, irq=51
e1000e: Intel(R) PRO/1000 Network Driver - 2.1.4-k
e1000e: Copyright(c) 1999 - 2012 Intel Corporation.
xemacps e000b000.ps7-ethernet: error in getting phy i/f
xemacps: probe of e000b000.ps7-ethernet failed with error -22
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
ULPI transceiver vendor/product ID 0x0451/0x1507
Found TI TUSB1210 ULPI transceiver.
ULPI integrity check: passed.
xusbps-ehci xusbps-ehci.0: Xilinx PS USB EHCI Host Controller
xusbps-ehci xusbps-ehci.0: new USB bus registered, assigned bus number 1
xusbps-ehci xusbps-ehci.0: irq 53, io mem 0x00000000
xusbps-ehci xusbps-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
mousedev: PS/2 mouse device common for all mice
i2c /dev entries driver
xadcps f8007100.ps7-xadc: Failed to request memory region
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: SDHCI controller on e0100000.ps7-sdio [e0100000.ps7-sdio] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
TCP: cubic registered
NET: Registered protocol family 17
VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
Registering SWP/SWPB emulation handler
dmatest: Started 1 threads using dma0chan0
dmatest: Started 1 threads using dma0chan1
dmatest: Started 1 threads using dma0chan2
dmatest: Started 1 threads using dma0chan3
dmatest: Started 1 threads using dma0chan4
mmc0: new high speed SDHC card at address 0007
mmcblk0: mmc0:0007 SD04G 3.70 GiB
dmatest: Started 1 threads using dma0chan5
mmcblk0: p1
dmatest: Started 1 threads using dma0chan6
dmatest: Started 1 threads using dma0chan7
List of all partitions:
1f00            1024 mtdblock0  (driver?)
1f01            5120 mtdblock1  (driver?)
1f02             128 mtdblock2  (driver?)
1f03            6016 mtdblock3  (driver?)
1f04            4096 mtdblock4  (driver?)
b300         3887104 mmcblk0  driver: mmcblk
  b301         3883008 mmcblk0p1 00000000-01
No filesystem could mount root, tried:  ext3 ext2 ext4 vfat msdos
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(1,0)

I think this statement in the log is the culprit

"INITRD: 0x1f8ca000+0x0028ac63 is not a memory region - disabling initrd"

I made all the necessary changes to the device tree to reserve memory for the Linux and the bare-metal application. I am quite sure that the issue is something to do with Uboot. Since when i run generate my BOOT.bin with the already generated file ( which comes with the design) It could boot in. Any help will be greatly appreciated.

Cheers,
Sun

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    I've read that v14.3build2 is still what you need to use. I did have some issues trying to use newer versions, but this one worked for me.

    Linux:
    https://github.com/Xilinx/linux-xlnx/archive/xilinx-14.3-build2.tar.gz

    U-boot:
    https://github.com/Xilinx/u-boot-xlnx/archive/xilinx-14.3-build2.tar.gz

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    There are some SD card issues with the xilinx-14.3 build of uboot, it is also mentioned in the xilinx wiki under known issues, hence i had to use a later version of uboot. Though i was able to solve this problem. it was because my Ram disk was getting copied outside the SDRAM region which Linux could see.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi there,

    in bootargs for devicetree, set console=ttyPS1 for ZedBoard!

    Ondrej