Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development PL to PS Interrupt disabling Ethernet Echo lwIP example
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 362 subscribers
  • Views 863 views
  • Users 0 members are here
Related

PL to PS Interrupt disabling Ethernet Echo lwIP example

e14 Contributor
e14 Contributor over 10 years ago

I'm using an interrupt from the PL to the PS from my custom IP that indicates data is ready to be read. I used code provided by AR #56446 to configure the interrupt in the SDK code. I'm getting the interrupt from the PL just fine, however enabling this interrupt in the way that I'm doing it seems to disable the Ethernet Echo functionality. I've isolated the issue to the interrupt configuration code. When I disable InitializeInterruptSystem () the Echo functionality comes back. BSP is the standard package created by the SDK for the example lwIP Echo project. Can someone please tell me what I'm doing wrong here?

InitializeInterruptSystem  is as below:

int InitializeInterruptSystem ( deviceID ) {

int Status;
 
GicConfig = XScuGic_LookupConfig ( deviceID );
if ( NULL == GicConfig ) {
return XST_FAILURE;
}
Status = XScuGic_CfgInitialize ( &InterruptController, GicConfig, GicConfig->CpuBaseAddress);
if ( Status != XST_SUCCESS ) {
return XST_FAILURE;
}
 
Status = SetUpInterruptSystem ( &InterruptController);
if ( Status != XST_SUCCESS ) {
return XST_FAILURE;
}
 
Status = XScuGic_Connect ( &InterruptController,
XPAR_FABRIC_AXI_DMA_0_S2MM_INTROUT_INTR,
(Xil_ExceptionHandler)InterruptHandler,
NULL);
/* Status = XScuGic_Connect ( &InterruptController,
XPAR_FABRIC_AXI_DMA_0_S2MM_INTROUT_INTR,
(Xil_InterruptHandler)InterruptHandler,
NULL);*/
XScuGic_Enable (&InterruptController, XPAR_FABRIC_AXI_DMA_0_S2MM_INTROUT_INTR);
 
// Initialize exception table and register the interrupt controller handler with exception table
Xil_ExceptionInit();
Xil_ExceptionRegisterHandler(XIL_EXCEPTION_ID_INT, (Xil_ExceptionHandler)XScuGic_InterruptHandler, &InterruptController);
 
// Enable non-critical exceptions
Xil_ExceptionEnable();
if ( Status != XST_SUCCESS ) {
return XST_FAILURE;
}
 
 
return XST_SUCCESS;
}
 
Thanks
Kavish
  • Sign in to reply
  • Cancel
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    Which lwIP Echo project are you referring to?  There are quite a few out there.

    The AR you posted was using non-Vivado tools.  I would suggest you start with checking what you have against AR58942:
    http://www.xilinx.com/support/answers/58942.html

    That is specifically for Zynq 7000 and Vivado, which using the Block Design (BD) makes it really easy to do.

    As for tracking the issue itself, I think I would start with checking that somewhere in the project there isn't already an interrupt definition.  I do not know which project you are using, so can only try to help guide you with this.  Is it possible you are re-defining the interrupt on accident to not be the echo interrupt?

    --Dan