Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development ADV7511 and PetaLinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 753 views
  • Users 0 members are here
Related

ADV7511 and PetaLinux

e14 Contributor
e14 Contributor over 9 years ago

Hello ladies and gentlemen,

 

recently I am trying to implement the reference design of the ADV7511 HDMI Controller to the ZedBoard (https://wiki.analog.com/resources/fpga/xilinx/kc705/adv7511). I was already able to build the Vivado project (Vivado 2015.4.2) successfully and run the test application provided by Analog Devices.

Now I am stuck though when trying to implement the design into a Linux built with PetaLinux 2016.4. I can build a PetaLinux around it and boot the image but no fb device was loaded. Also I adjusted the kernel config as far as it was possible for me and I let PetaLinux handle the devicetree.

Is there something I have to take care of before I can actually run a Linux built with PetaLinux which can successfully load a fb-device for the ADV7511?

 

Alternatively I tried following this guide (http://blog.idv-tech.com/2014/05/25/hdmi-on-zedboard-with-petalinux/) to build my image as far as possible. He used the official Analog Devices Kernel and their configs to run the design, but for some reason I get crash when I try to petalinux-build:

INFO: Checking component...
INFO: Generating make files and build linux
INFO: Generating make files for the subcomponents of linux
INFO: Building linux
[INFO ] pre-build linux/rootfs/fwupgrade
[INFO ] pre-build linux/rootfs/peekpoke
[INFO ] build system.dtb
[INFO ] build linux/kernel
[ERROR] make[3]: *** [prepare3] Error 1
[ERROR] make[2]: *** [sub-make] Error 2
[ERROR] make[1]: *** [/[...]/build/linux/kernel/analogdevices-kernel/vmlinux] Error 2
ERROR: Failed to build linux

 

Appreciate any tips that will help me advance in that project.

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Bunga65,

    When you used http://blog.idv-tech.com/2014/05/25/hdmi-on-zedboard-with-petalinux/ in attempt to build your petalinux, did you use petalinx 2013.10 and Vivado 2013.4? If not then try running through it using those tools.

    Also, if this is for educational purposes then please ask any further questions over at the Digilent forum as they are the main point of contact for educational support. https://forum.digilentinc.com/

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Bunga65,

    When you used http://blog.idv-tech.com/2014/05/25/hdmi-on-zedboard-with-petalinux/ in attempt to build your petalinux, did you use petalinx 2013.10 and Vivado 2013.4? If not then try running through it using those tools.

    Also, if this is for educational purposes then please ask any further questions over at the Digilent forum as they are the main point of contact for educational support. https://forum.digilentinc.com/

    --Josh