Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development GPIOs
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 295 views
  • Users 0 members are here
Related

GPIOs

e14 Contributor
e14 Contributor over 12 years ago

Hi, I am trying to interface a device through GPIOs numbered 11 and 12. I am communicating with my device using a simple UART protocol using Rx and Tx.

I have to communicate hex data frames serially to my device in order to get what I need from it. The problem is that I can configure the outputs of these GPIO pins in /sys/class/gpio/gpioxx/value and set the value to be zero or one.

Now is there a way I can send bytes and words serially without setting and un-setting each bit ( I am translating my hex frames to binary and setting the values of the pin using a shell script sequentially in order). 

Also please suggest a way I can use to transfer the data using a custom baud rate.   

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    If you want to send bytes as opposed to 'bit banging' the RX/TX interface then use one of the available UART IP, such as the axi_uartlite:

    http://www.xilinx.com/support/documentation/ip_documentation/axi_uartlite/v1_02_a/axi_uartlite_ds741.pdf

     

    If you want more options you can use the second hardware uart in the Zynq PS (Processing System) or use the axi Uart16550 IP:

    http://www.xilinx.com/support/documentation/ip_documentation/axi_uart16550/v2_0/pg143-axi-uart16550.pdf

     

    You can set a custom baud rate with any ot these uarts.

     

    -Gary