Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development BOOT.bin creation for Linux 2017.2 BSP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 349 views
  • Users 0 members are here
Related

BOOT.bin creation for Linux 2017.2 BSP

100docjay
100docjay over 8 years ago
I have the 2017.2 BSP for the ultrazed.  The prebuilt linux images boot correctly - when I use the supplied BOOT_SD.bin (renamed to BOOT.bin, and related system.dtb image.ub files that are supplied.
 
  
   

 
     I want to use my own .bit file with the supplied files, but when I create a BOOT.bin using the SDK it does not boot.  When I power on (with the SD media inserted) it does say: Xilinx Zynq MP First Stage Boot Loader Release 2017.2 ....  However it never gets to uboot or any further for that matter.
     I have followed the same procedure that has worked in the past for the picoZed board.
     Can someone provide any details on how to create the boot.bin file for this release?  What am I doing wrong.  Is there any tutorial that covers creating the boot.bin file for a linux based ultrazed system?

  
 
  • Sign in to reply
  • Cancel
  • narrucmot
    0 narrucmot over 8 years ago

    Instead of using the SDK, you may have more success creating the BOOT.BIN from from the Linux command line.  It may also help to take a loot at the scripts in the Avnet github repository for (https://github.com/Avnet/petalinux).  In particular, the PetaLinux BSP script for the UltraZed (https://github.com/Avnet/petalinux/blob/master/scripts/make_uz3eg_petalinux_bsp.sh).

    When run from the PetaLinux project folder, the PetaLinux command to create the boot.bin file looks like this:

    petalinux-package --boot --fsbl images/linux/<name_of_FSBL_elf_file> --fpga <path_to_PL_bitstream> --uboot --force

     

    I hope this helps.

    Cheers!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100docjay
    0 100docjay over 8 years ago in reply to narrucmot

    OK, thanks.  I will try that.