Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development QEMU - Deep Dive
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 364 subscribers
  • Views 661 views
  • Users 0 members are here
Related

QEMU - Deep Dive

e14 Contributor
e14 Contributor over 14 years ago

I have written a blog post detailing the QEMU environment available from Xilinx.

http://zynqgeek.blogspot.com/2012/10/qemu-deep-dive.html

Enjoy!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Two questions from the blog:

    (1) QEMU Xilinx ARM emulate NEON Instruction ?
    (2) QEMU Xilinx ARM emulate double precision FPU ?

    If you dive into the source code of qemu, specifically within the qemu git repo here:

    git://git.xilinx.com/qemu-xarm.git

    within the target-arm folder there is a file called translate.c.  Within this file there is a function called disas_neon_data_insn().  This handles the NEON instruction decoding.

    As for the double precision, I see no reason why it would not, as the ARM emulation should be operationally equivalent.

    I have a post about linpack performance on the Zedboard, I'll see if I can write a quick follow up about the performance in qemu - that will confirm the double precision float using the NEON core.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Two questions from the blog:

    (1) QEMU Xilinx ARM emulate NEON Instruction ?
    (2) QEMU Xilinx ARM emulate double precision FPU ?

    If you dive into the source code of qemu, specifically within the qemu git repo here:

    git://git.xilinx.com/qemu-xarm.git

    within the target-arm folder there is a file called translate.c.  Within this file there is a function called disas_neon_data_insn().  This handles the NEON instruction decoding.

    As for the double precision, I see no reason why it would not, as the ARM emulation should be operationally equivalent.

    I have a post about linpack performance on the Zedboard, I'll see if I can write a quick follow up about the performance in qemu - that will confirm the double precision float using the NEON core.