Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Audio IC configuration Error!
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 296 views
  • Users 0 members are here
Related

Audio IC configuration Error!

e14 Contributor
e14 Contributor over 13 years ago

Hi,

While adding adau1716 i am getting the following error


CC sound/soc/codecs/adau1761.c: In function 'adau1761_setup_digmic_jackdetect'


sound/soc/codecs/adau1761.c:498:3: error: implicit declaration of function 'snd_soc_add_controls' [-Werror=implicit-function-declaration]
sound/soc/codecs/adau1761.c: At top level:
sound/soc/codecs/adau1761.c:396:12: warning: 'adau1761_is_slave_mode' defined but not used [-Wunused-function]
cc1: some warnings being treated as errors

make[3]: *** [sound/soc/codecs/adau1761.o] Error 1
make[2]: *** [sound/soc/codecs] Error 2
make[1]: *** [sound/soc] Error 2
make: *** [sound] Error 2

Attached also a snapshot of the same.
Kindly help with the workaround.

Thanks,
Ved


  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hi,
    We have fixed the driver issue but getting the following message relating to process termination.

    In the Alsa Mixer, i am able to see dummy and loopback as below. In the Alsa Mixer what device name should i expect?

    "


    root@localhost:~# dmesg |grep sound

    [    5.520000] init_stage2: zedboard-sound main process (1345) terminated with status 255



    root@localhost:~# arecord --list-devices
    **** List of CAPTURE Hardware Devices ****
    card 0: Dummy [Dummy], device 0: Dummy PCM [Dummy PCM]
      Subdevices: 8/8
      Subdevice #0: subdevice #0
      Subdevice #1: subdevice #1
      Subdevice #2: subdevice #2
      Subdevice #3: subdevice #3
      Subdevice #4: subdevice #4
      Subdevice #5: subdevice #5
      Subdevice #6: subdevice #6
      Subdevice #7: subdevice #7
    card 1: Loopback [Loopback], device 0: Loopback PCM [Loopback PCM]
      Subdevices: 8/8
      Subdevice #0: subdevice #0
      Subdevice #1: subdevice #1
      Subdevice #2: subdevice #2
      Subdevice #3: subdevice #3
      Subdevice #4: subdevice #4
      Subdevice #5: subdevice #5
      Subdevice #6: subdevice #6
      Subdevice #7: subdevice #7
    card 1: Loopback [Loopback], device 1: Loopback PCM [Loopback PCM]
      Subdevices: 8/8
      Subdevice #0: subdevice #0
      Subdevice #1: subdevice #1
      Subdevice #2: subdevice #2
      Subdevice #3: subdevice #3
      Subdevice #4: subdevice #4
      Subdevice #5: subdevice #5
      Subdevice #6: subdevice #6
      Subdevice #7: subdevice #7


    root@localhost:~# cat /proc/asound/devices
      0: [ 0]   : control
    16: [ 0- 0]: digital audio playback
    24: [ 0- 0]: digital audio capture
    32: [ 1]   : control
    33:        : timer
    48: [ 1- 0]: digital audio playback
    49: [ 1- 1]: digital audio playback
    56: [ 1- 0]: digital audio capture
    57: [ 1- 1]: digital audio capture

    Card: Dummy                                          F1:  Help               u00A6
    u00A6 Chip: Dummy Mixer                                    F2:  System information u00A6
    u00A6 View: F3:[Playback] F4: Capture  F5: All             F6:  Select sound card  u00A6
    u00A6 Item: Master [dB gain: 0.00, 0.00]                   Esc: Exit               u00A6
    u00A6                                                                              u00A6
    u00A6                   +--+     +--+     +--+     +--+     +--+                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6   +----- Sound Card ------+    u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6   u00A6-  (default)           u00A6    u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6   u00A60  Dummy               u00A6    u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6   u00A61  Loopback            u00A6    u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6   u00A6   enter device name...u00A6    u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6   +-----------------------+    u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6     u00A6u00A6u00A6u00A6                   u00A6
    u00A6                   +--+     +--+     +--+     +--+     +--+                   u00A6
    u00A6                 100<>100 100<>100 100<>100 100<>100 100<>100                 u00A6
    u00A6                < Master > Synth     Line      CD      Mic                    u00A6



    u00A6                                                             
    "

    kindly help.
    Thanks,
    ved