Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Crash loading Ramdisk
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 813 views
  • Users 0 members are here
Related

Crash loading Ramdisk

suppamax
suppamax over 11 years ago

Hi,

I have the following setup:

HW:
board: microzed + FMC carrier + FMCOMMS3
RTL: I took the reference design from here
http://wiki.analog.com/resources/fpga/docs/hdl
and ported it to microzed, remapping pins and removing unnecessary ports (i.e HDMI).

SW:
I got linux from
https://github.com/analogdevicesinc/linux
For the devicetree I used zynq-zed-adv7511-ad9361-fmcomms2-3.dts, also from ADI's linux distribution
The ramdisk is the one provided by Xilinx.

During boot I get

## Booting kernel from Legacy Image at 02080000 ...
   Image Name:   Linux-4.0.0-g86cfd8d
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3331976 Bytes = 3.2 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 04000000 ...
   Image Name:  
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    5309954 Bytes = 5.1 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 02000000
   Booting using the fdt blob at 0x2000000
   Loading Kernel Image ... OK
   Loading Ramdisk to 1faef000, end 1ffff602 ...

and the boot hangs.

Could you help with this issue?


Thanks,
Max

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi Max,

    It was not clear to me from OP that you had already ruled out any differences in U-Boot and that you have already narrowed this down to only differences in the Programmable Logic design.

    One thing to check within the HDL is to verify that the address mapping between your MicroZed ported design and the original design for say ZedBoard.  If the memory assignments for the PL blocks on the AXI interconnects does not match the DTS, this could definitely cause a lockup during Linux boot.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • suppamax
    0 suppamax over 11 years ago in reply to zedhed

    Hi Kevin,

    I'm not 100% sure that the problem is in HDL - that was my feeling, after the tests I described you.

    Anyway, I checked in the address editor that the base addresses are the same as in the original design: they match.
    Is there something more I shall check?

    I also tried to follow your suggestion about uboot.
    I copied linaro in the rootfs partition of the SD card (it was empty before since I don't really need it) and booted using

    tftpboot 0x3000000 uImage && tftpboot 0x2A00000 devicetree.dtb && tftpboot 0x2000000 uramdisk.image.gz
    bootm 0x3000000 - 0x2A00000

    As a result I get

    Internal error: : 406 [#1] PREEMPT SMP ARM
    [...]
    Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • suppamax
    0 suppamax over 11 years ago in reply to zedhed

    Hi Kevin,

    I'm not 100% sure that the problem is in HDL - that was my feeling, after the tests I described you.

    Anyway, I checked in the address editor that the base addresses are the same as in the original design: they match.
    Is there something more I shall check?

    I also tried to follow your suggestion about uboot.
    I copied linaro in the rootfs partition of the SD card (it was empty before since I don't really need it) and booted using

    tftpboot 0x3000000 uImage && tftpboot 0x2A00000 devicetree.dtb && tftpboot 0x2000000 uramdisk.image.gz
    bootm 0x3000000 - 0x2A00000

    As a result I get

    Internal error: : 406 [#1] PREEMPT SMP ARM
    [...]
    Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b