Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Crash loading Ramdisk
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 364 subscribers
  • Views 811 views
  • Users 0 members are here
Related

Crash loading Ramdisk

suppamax
suppamax over 11 years ago

Hi,

I have the following setup:

HW:
board: microzed + FMC carrier + FMCOMMS3
RTL: I took the reference design from here
http://wiki.analog.com/resources/fpga/docs/hdl
and ported it to microzed, remapping pins and removing unnecessary ports (i.e HDMI).

SW:
I got linux from
https://github.com/analogdevicesinc/linux
For the devicetree I used zynq-zed-adv7511-ad9361-fmcomms2-3.dts, also from ADI's linux distribution
The ramdisk is the one provided by Xilinx.

During boot I get

## Booting kernel from Legacy Image at 02080000 ...
   Image Name:   Linux-4.0.0-g86cfd8d
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    3331976 Bytes = 3.2 MiB
   Load Address: 00008000
   Entry Point:  00008000
   Verifying Checksum ... OK
## Loading init Ramdisk from Legacy Image at 04000000 ...
   Image Name:  
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    5309954 Bytes = 5.1 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 02000000
   Booting using the fdt blob at 0x2000000
   Loading Kernel Image ... OK
   Loading Ramdisk to 1faef000, end 1ffff602 ...

and the boot hangs.

Could you help with this issue?


Thanks,
Max

  • Sign in to reply
  • Cancel
Parents
  • suppamax
    0 suppamax over 11 years ago

    I was also wandering...
    Linux has been provided by ADI and the ramdisk by Xilinx: is it possible that they're not compatible or something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • suppamax
    0 suppamax over 11 years ago

    I was also wandering...
    Linux has been provided by ADI and the ramdisk by Xilinx: is it possible that they're not compatible or something?