Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Building Open Source Linux from the linux-xlnx, hangs when booting.
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 574 views
  • Users 0 members are here
Related

Building Open Source Linux from the linux-xlnx, hangs when booting.

e14 Contributor
e14 Contributor over 12 years ago

Hello.

After extensive testing and google/(xilinx forum)/(microzed) searching, I decided to post this question here.


I'm trying to cross-compile the linux kernel (Open Source Linux from Xilinx) in an OpenSUSE computer and boot it in a MicroZed board. I downloaded the Vivado Web Pack and the linux kernel (what I think is "Open Source Linux") from the xilinx's linux-xlnx git repository. I build the kernel, and it generates the image. For this, I had to generate build the mkimage utility found in the "u-boot-xlnx" file that also comes in the repository, as outlined in the Xilinx's guide.


For the cross-compilation process, I use the cross-compilation toolchain that are available after installing Vivado and sourcing the settings64.sh file. I copy the uImage to an SD card. In this card, there are also the other booting files and images from the MicroZed SD image. That is, I use the same boot.bin, the ramdisk, etc., and I only replace the uImage that I just cross-compiled.


The kernel is able to boot, but it hangs, in the line that says:


"Starting Kernel ...."



The checksums and everything prior to that is ok.



It simply hangs there, and no further action is performed. One reason may be that it is not decompressing the uImage properly because I might be using the wrong mkimage utility.



Any thoughts on what could it be and how to procceed?



Good day.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I haven't done anything with SuSe, but I know there are differences in the way the development environment is set up between CentOS and Ubuntu.  Although my first thought is that there may be something missing in your SuSe setup, I would expect to see some kind of error in the compilation process.  Assuming the compilation is clean, here are some things I can think of to try to track this down:

    1. SuSe development environment issue.  Have you tried replicating the kernel build using a CentOS or Ubuntu development environment?  Just as a sanity check to verify all the procedures you are using are correct?  See the Ubuntu tutorial on Zedboard.org for information on creating a development environment based on either distribution.

    2. Mismatch between u-boot in boot.bin and the kernel version in the uImage.  This seems unlikely, but the boot is hanging at a very early stage in the kernel boot.  You may want to try rebuilding the corresponding version of u-boot for the tag you are using for the kernel, then substitute that in the boot.bin file to see if there is any change.

    2. Configuration error in the Linux kernel.  If you are unable to complete 1 above to verify your process, then this may be relevant. 

    3. Error in the compiled device tree.  Unlikely to be the problem at this stage of the boot, but anything is possible. 

    I know there are quite a few developers out there, particularly in Europe, using SuSe, so if anyone has some actual similar experience, please feel free to jump in here.

    Let me know the results if you try any of the suggestions above.  We may need additional information to get to the bottom of this.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I haven't done anything with SuSe, but I know there are differences in the way the development environment is set up between CentOS and Ubuntu.  Although my first thought is that there may be something missing in your SuSe setup, I would expect to see some kind of error in the compilation process.  Assuming the compilation is clean, here are some things I can think of to try to track this down:

    1. SuSe development environment issue.  Have you tried replicating the kernel build using a CentOS or Ubuntu development environment?  Just as a sanity check to verify all the procedures you are using are correct?  See the Ubuntu tutorial on Zedboard.org for information on creating a development environment based on either distribution.

    2. Mismatch between u-boot in boot.bin and the kernel version in the uImage.  This seems unlikely, but the boot is hanging at a very early stage in the kernel boot.  You may want to try rebuilding the corresponding version of u-boot for the tag you are using for the kernel, then substitute that in the boot.bin file to see if there is any change.

    2. Configuration error in the Linux kernel.  If you are unable to complete 1 above to verify your process, then this may be relevant. 

    3. Error in the compiled device tree.  Unlikely to be the problem at this stage of the boot, but anything is possible. 

    I know there are quite a few developers out there, particularly in Europe, using SuSe, so if anyone has some actual similar experience, please feel free to jump in here.

    Let me know the results if you try any of the suggestions above.  We may need additional information to get to the bottom of this.

    Ron