Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Boot runs only partial application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 350 views
  • Users 0 members are here
Related

Boot runs only partial application

e14 Contributor
e14 Contributor over 9 years ago

Hello,

I am a newbie to the Zedboard. I am following the SW & HW labs provided by Xilinx. The pre-defined templates like the HelloWorld, MemoryTests, PeripheralTests etc seem to work fine on the Debug Build Configuration. However, when I tried to change the build configuration to Release(Active) from Lab6 & Lab7, the board doesn't seem to execute the complete application. I tried running the MemoryTests & PeripheralTests from Lab6 booting from the QSPI single, after programming it. The applications gets stuck @ "Running Interrupt Test  for ps7_ethernet_0..." for peripheral tests and no messages are printed for memory_tests, probably stuck at the beginning itself.

 

 

Kindly provide some insights to the issue.

Software Used

Vivado Design Suite 2015.3

 

Hardware

Default Zynq hdf

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Fadilluquman,

    Are you refering to the hardware/software labs located at this location? http://zedboard.org/support/trainings-and-videos

    If so which lab version did you download? As you can see we only offer tutorials that support Vivado 2013.3/2014.4.1/2015.2/2016.2.

    On another note if you look at a the 2016.2 lab documents, you will notice that we skipped the changing the build configurations to release(Active). The reason we did this is due to the issue you are currently encountering. This issue is caused by a bug with the tools that should have been fixed in the Vivado 2016.3 release. However I have not confirmed that fix myself.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Fadilluquman,

    Are you refering to the hardware/software labs located at this location? http://zedboard.org/support/trainings-and-videos

    If so which lab version did you download? As you can see we only offer tutorials that support Vivado 2013.3/2014.4.1/2015.2/2016.2.

    On another note if you look at a the 2016.2 lab documents, you will notice that we skipped the changing the build configurations to release(Active). The reason we did this is due to the issue you are currently encountering. This issue is caused by a bug with the tools that should have been fixed in the Vivado 2016.3 release. However I have not confirmed that fix myself.

    --Josh