Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Copying files in zedboard memory!
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 365 views
  • Users 0 members are here
Related

Copying files in zedboard memory!

e14 Contributor
e14 Contributor over 12 years ago

I am trying to make a file accessible for zedboard. I have a .wav file which using an C code I can transform in binary data which are saved afterwards in the Zedboard memory. But the problem is that in order to run the C code I have to have the .wav file accessible from the C code. When I run the code in Zedboard I can not acces my file which reside in my PC. I tried to put both the code and the .wav file in SD card and to run the zedboard but it doesn't work since it can not access the file.

Any help can be appreciated.

Regards,
Jet

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Is this a 'stand alone' application or one running under an Operating System (i.e. Linux)?

     

    Also which version of the Xilinx tools are you using?

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Hi Gary,

    I am using SDK 2013.2 and yes it is stand alone application. I was using the "no-os" design for zedboard and fmcomms2 provided by analog devices.

    Any idea for the first comment!?

    Regards,
    jet