Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development How to flush the buffer in burst mode
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 527 views
  • Users 0 members are here
Related

How to flush the buffer in burst mode

rtenas
rtenas over 8 years ago

I am using the ZedBoard and FMCOMMS3 to receive data in two channels (I am programming with Matlab). I am using an IF of 25KHz and Fs of 2 MHz. Since I get a warining : "1 samples from the radio have been lost", I am trying to use the burst mode. When I do that, I do not lose samples any more, since they are stored in the buffer and then processed. The problem is that I want to measure in real-time. I am processing the next example:

1. I send a -50 dBm signal with a signal generator to the zedboard and I capture the data.

2. I change the output power of the signal generator to -40 dBm. I capture the data, and I expect to get this -40 dBm, but I still get -50 dBm because the buffer was filled with the previous signal.

Is there a way to flush the buffer of the sdrrx object before capturing the new set of data (-40 dBm) in the burst mode?

The other option if to use the normal mode, without burst mode enabled, but in that way I lose samples and I guess that in that way I can not completely trust the phase stimation I get from the signal.

  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello,

    For educational support please ask all zedboard related questions at the Digilent Support forum.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer