Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development which embedded linux development environment
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 363 subscribers
  • Views 390 views
  • Users 0 members are here
Related

which embedded linux development environment

100padudle
100padudle over 12 years ago

Hello,

I am writing some application software for a MicroZed SOM module.  I need to provide a command line and web interface for controlling some hardware so I am planning to use some flavor of linux on the Arm processors of the Zynq.

There are quite a few ways to boot and run linux on the Zynq. I am looking for the approach that is most convenient with respect to development and deployment.

At this point I have read every website I can find on the subject. These howto's and tutorials generally take three different approaches.

1. u-boot -> linux kernel + ramdisk root filesystem
2. u-boot -> linux kernel + sd card Ubuntu root filesystem
3. Petalinux semi-proprietary flow.

Approach 1 boots fast and is very stable but is not convenient for development.  It looks like every development cycle requires you to cross-compile, compress the ramdisk image, write the ramdisk image to the sd card and reboot the MicroZed.

Approach 2 seems like a lot of overhead to carry forward to deployment. On the other hand it should be possible to ssh into the MicroZed and edit-compile-run very quickly. Code changes would be persistent due to the SD card filesystem.

Approach 3 I have not tried.

What do people here use for linux application development on Zed?  Is there an intermediate way to run linux that provides ssh, vim, gcc but mounts an sd card or NFS persistent filesystem?

What do people here prefer as a development environment for relatively simple applications?

  Pete

  • Sign in to reply
  • Cancel
Parents
  • 100padudle
    0 100padudle over 12 years ago

    I have made a little progress booting ubuntu on the microzed.

    I am using this root filesystem.
    http://releases.linaro.org/12.09/ubuntu/precise-images/ubuntu-desktop/linaro-precise-ubuntu-desktop-20120923-436.tar.gz

    I had to change the configuration settings on the linux kernel to turn off CPU_FREQ. That fork can be found here.
    https://github.com/hdlguy/linux-xlnx.git

    Since several of us will be developing on the same network we had to change the hostname on our individual microzeds and then modify the MAC address in the u-boot parameter space.

    Now all is good. We can run apt-get to get applications. We can collaborate accross the network using git and svn.

    The only negative of this approach is the size of the filesystem. Copying that filesystem to a slow SD card is tedious.  Also, differences in the file system will occur between development boards.

      Pete

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • 100padudle
    0 100padudle over 12 years ago

    I have made a little progress booting ubuntu on the microzed.

    I am using this root filesystem.
    http://releases.linaro.org/12.09/ubuntu/precise-images/ubuntu-desktop/linaro-precise-ubuntu-desktop-20120923-436.tar.gz

    I had to change the configuration settings on the linux kernel to turn off CPU_FREQ. That fork can be found here.
    https://github.com/hdlguy/linux-xlnx.git

    Since several of us will be developing on the same network we had to change the hostname on our individual microzeds and then modify the MAC address in the u-boot parameter space.

    Now all is good. We can run apt-get to get applications. We can collaborate accross the network using git and svn.

    The only negative of this approach is the size of the filesystem. Copying that filesystem to a slow SD card is tedious.  Also, differences in the file system will occur between development boards.

      Pete