Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Can't start x in xillinux
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 363 subscribers
  • Views 411 views
  • Users 0 members are here
Related

Can't start x in xillinux

e14 Contributor
e14 Contributor over 13 years ago

After I entered "startx" in xillinux, vga output goes black, and linux not response my input anymore.
I'm trying to write some driver modules for axi_gpio, but I didn't install any mmodule or driver.
Also "startx" goes well yesterday.
I'm "startx" from serial port and recorded the output bleow. Hope someone will solve the problem, or I may reinstall the xillinux...


  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    U-Boot 2012.04.01 (Oct 16 2012 - 17:41:50)



    DRAM:  512 MiB

    WARNING: Caches not enabled

    MMC:   SDHCI: 0

    Using default environment



    In:    serial

    Out:   serial

    Err:   serial

    Net:   zynq_gem

    Hit any key to stop autoboot:  0

    Copying Linux from SD to RAM...

    Device: SDHCI

    Manufacturer ID: 2

    OEM: 544d

    Name: SD08G

    Tran Speed: 25000000

    Rd Block Len: 512

    SD version 2.0

    High Capacity: Yes

    Capacity: 7.5 GiB

    Bus Width: 4-bit

    reading zImage



    2676424 bytes read

    reading devicetree.dtb



    6062 bytes read

    reading ramdisk8M.image.gz



    ** Unable to read "ramdisk8M.image.gz" from mmc 0:1 **

    ## Starting application at 0x00008000 ...

    Uncompressing Linux... done, booting the kernel.

    [    0.000000] Booting Linux on physical CPU 0


    [    0.000000] Linux version 3.3.0-xillinux-1.0+ (eli@ocho.localdomain) (gcc ver
    sion 4.5.1 (Sourcery G++ Lite 2010.09-62) ) #2 SMP PREEMPT Wed Oct 17 17:09:20 I
    ST 2012


    [    0.000000] CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d


    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instructio
    n cache


    [    0.000000] Machine: Xilinx Zynq Platform, model: Xillinux for Zedboard


    [    0.000000] bootconsole [earlycon0] enabled


    [    0.000000] Memory policy: ECC disabled, Data cache writealloc


    [    0.000000] BUG: mapping for 0xf8f00000 at 0xfe00c000 out of vmalloc space


    [    0.000000] BUG: mapping for 0xe0000000 at 0xfe000000 out of vmalloc space


    [    0.000000] BUG: mapping for 0xffff1000 at 0xfe200000 out of vmalloc space


    [    0.000000] PERCPU: Embedded 7 pages/cpu @c09c5000 s5440 r8192 d15040 u32768


    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pag
    es: 125824


    [    0.000000] Kernel command line: consoleblank=0 root=/dev/mmcblk0p2 rw rootwa
    it earlyprintk


    [    0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes)


    [    0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)


    [    0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)


    [    0.000000] Memory: 240MB 256MB = 496MB total


    [    0.000000] Memory: 497408k/497408k available, 26880k reserved, 0K highmem


    [    0.000000] Virtual kernel memory layout:


    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)


    [    0.000000]     fixmap  : 0xfff00000 - 0xfffe0000   ( 896 kB)


    [    0.000000]     vmalloc : 0xe0800000 - 0xfd000000   ( 456 MB)


    [    0.000000]     lowmem  : 0xc0000000 - 0xe0000000   ( 512 MB)


    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)


    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)


    [    0.000000]       .text : 0xc0008000 - 0xc04c553c   (4854 kB)


    [    0.000000]       .init : 0xc04c6000 - 0xc04ef540   ( 166 kB)


    [    0.000000]       .data : 0xc04f0000 - 0xc0521ea0   ( 200 kB)


    [    0.000000]        .bss : 0xc0521ec4 - 0xc053df68   ( 113 kB)


    [    0.000000] Preemptible hierarchical RCU implementation.


    [    0.000000]  Verbose stalled-CPUs detection is disabled.


    [    0.000000] NR_IRQS:128


    [    0.000000] xlnx,ps7-ttc-1.00.a #0 at 0xe0800000, irq=43


    [    0.000000] Console: colour dummy device 80x30


    [    0.000000] console [tty0] enabled, bootconsole disabled




    Ubuntu 12.04 LTS localhost.localdomain ttyPS0



    localhost login: root (automatic login)



    Last login: Thu Jan  1 00:00:06 UTC 1970 on tty1

    Welcome to the Xillinux distribution for Zynq-7000 EPP.



    You may communicate data with standard FPGA FIFOs in the logic fabric by

    writing to or reading from the /dev/xillybus_* device files. Additional

    pipe files of that sort can be set up at request of a custom Xillybus IP core.



    For more information: http://www.xillybus.com.



    To start a graphical X-Windows session, type "startx" at shell prompt.



    sroot@localhost:~# startx

    hostname: Name or service not known

    xauth:  error in locking authority file /root/.Xauthority

    xauth:  error in locking authority file /root/.Xauthority





    X.Org X Server 1.11.3

    Release Date: 2011-12-16

    X Protocol Version 11, Revision 0

    Build Operating System: Linux 2.6.38-1209-omap4 armv7l Ubuntu

    Current Operating System: Linux localhost.localdomain 3.3.0-xillinux-1.0+ #2 SMP
    PREEMPT Wed Oct 17 17:09:20 IST 2012 armv7l

    Kernel command line: consoleblank=0 root=/dev/mmcblk0p2 rw rootwait earlyprintk

    Build Date: 05 April 2012  12:04:28AM

    xorg-server 2:1.11.4-0ubuntu10 (For technical support please see http://www.ubun
    tu.com/support)

    Current version of pixman: 0.24.4

            Before reporting problems, check http://wiki.x.org

            to make sure that you have the latest version.

    Markers: (--) probed, (**) from config file, (==) default setting,

            (++) from command line, (!!) notice, (II) informational,

            (WW) warning, (EE) error, (NI) not implemented, (??) unknown.

    (==) Log file: "/var/log/Xorg.0.log", Time: Thu Jan  1 00:00:11 1970

    (==) Using system config directory "/usr/share/X11/xorg.conf.d"

    Invalid MIT-MAGIC-COOKIE-1 keyInvalid MIT-MAGIC-COOKIE-1 key


    waiting for X server to begin accepting connections .

    Invalid MIT-MAGIC-COOKIE-1 keyInvalid MIT-MAGIC-COOKIE-1 key..

    Invalid MIT-MAGIC-COOKIE-1 keyInvalid MIT-MAGIC-COOKIE-1 key..

    Invalid MIT-MAGIC-COOKIE-1 keyInvalid MIT-MAGIC-COOKIE-1 key..

    Invalid MIT-MAGIC-COOKIE-1 keyInvalid MIT-MAGIC-COOKIE-1 key..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    The by far most common reason for this problem is a faulty SD card. Please use a Sandisk if you aren't doing so already.

       Eli