Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development LED application on Zed board
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 363 subscribers
  • Views 2176 views
  • Users 0 members are here
Related

LED application on Zed board

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I am working on Zed board. I would like to work on the eclipse based SDK to dump the basic bare-metal applications onto Zed the board. I am able to put the hello world application through JTAG, where the "Hello World" text gets printed through the serial port. This is the process I follow to get the hello world application deployed on the target:
1. Import the system.xml file into the eclipse based Xilinx SDK IDE.
2. Create a new application project, with support of an existing standalone bsp.
3. The application project is created with a hello world template.
4. Now, compile and Run the application project onto the target, with the target configured in JTAG mode.
With these steps, the "Hello World" text gets printed on the serial port of the target.

Following the above steps, I am not able to work on the LED application. It seems like there are some hardware initialization missing in the process, which is the reason why the application fails. How do I put the hardware configuration file on the target board ? Do I need to use Impact tool for making the basic LED example work on the Zed platform.
I am pretty new to the FPGA part of programming, but fine with ARM side bare-metal applications.

Thank You

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Let me suggest that you move to the current Vivado tool suite. You will find more current examples and support for the Zynq device.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Let me suggest that you move to the current Vivado tool suite. You will find more current examples and support for the Zynq device.

     

    -Gary