Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development Xillinux issue with startx
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 363 subscribers
  • Views 1251 views
  • Users 0 members are here
Related

Xillinux issue with startx

e14 Contributor
e14 Contributor over 14 years ago

I have tried the Xillinux example with Ubuntu
I get the login right, but when I try startx i get the following error:

root@localhost:~# startx
hostname: Name or service not known
xauth: (stdin):1:  bad display name "localhost.localdomain:0" in "add" command


X.Org X Server 1.11.3
Release Date: 2011-12-16
X Protocol Version 11, Revision 0
Build Operating System: Linux 2.6.38-1209-omap4 armv7l Ubuntu
Current Operating System: Linux localhost.localdomain 3.3.0-xillinux-1.0+ #2 SMP PREEMPT Wed Oct 17 17:09:20 IST 2012 armv7l
Kernel command line: consoleblank=0 root=/dev/mmcblk0p2 rw rootwait earlyprintk
Build Date: 05 April 2012  12:04:28AM
xorg-server 2:1.11.4-0ubuntu10 (For technical support please see http://www.ubuntu.com/support)
Current version of pixman: 0.24.4
        Before reporting problems, check http://wiki.x.org
        to make sure that you have the latest version.
Markers: (--) probed, (**) from config file, (==) default setting,
        (++) from command line, (!!) notice, (II) informational,
        (WW) warning, (EE) error, (NI) not implemented, (??) unknown.
(==) Log file: "/var/log/Xorg.0.log", Time: Thu Jan  1 00:14:24 1970
(==) Using system config directory "/usr/share/X11/xorg.conf.d"
Parse error on line 2 of section (null) in file /usr/share/X11/xorg.conf.d/10-evdev.conf
        "
         5u00A7
          (
           " is not a valid keyword in this section.
(EE) Problem parsing the config file
(EE) Error parsing the config file

Fatal server error:
no screens found

Please consult the The X.Org Foundation support
         at http://wiki.x.org
for help.
Please also check the log file at "/var/log/Xorg.0.log" for additional information.

ddxSigGiveUp: Closing log
Server terminated with error (1). Closing log file.
xinit: giving up
xinit: unable to connect to X server: No such file or directory
xinit: server error
xauth: (argv):1:  bad display name "localhost.localdomain:0" in "remove" command
root@localhost:~#

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hello!

    Yes, I have some problems after that errors. Some programs fails to start. X server fails to start.
    I have 2 stock SD card. One card is better but on both of them sometimes such errors occur.
    I will try use Sandisk SD!

    thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Hello!

    Yes, I have some problems after that errors. Some programs fails to start. X server fails to start.
    I have 2 stock SD card. One card is better but on both of them sometimes such errors occur.
    I will try use Sandisk SD!

    thank you!