Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
Software Application Development MicroZed Run sdk application
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 364 subscribers
  • Views 1062 views
  • Users 0 members are here
Related

MicroZed Run sdk application

raymadigan
raymadigan over 10 years ago

I bought a MicroZed a long time ago and am finally getting to it.  I have built an application following the Adam Taylor blog to write Hello World to the console.  I have build the application and it seems ok, but I can't get it to run. 

At first I got a message that there was no ARM device on connection local. Cable is not connected to host.

I have created a Target connection to connect to the device:

Type:  Hardware Server
Host:  192.168.1.10
Port: 3121

I get the message that the hardware server is not running on the machine.  I can't find the hardware server to run it.  On some pages I found while googling I found where I was told to run hw_server but that doesn't exist anymore.

What did I miss?  I will work to figure this out, I just need a pointer.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Do you have a JTAG programming cable, such as an HS3 cable connected to your MicroZed?

    http://www.em.avnet.com/en-us/design/drc/Pages/Digilent-JTAG-HS3-Programming-Cable.aspx

     

    You connect this cable directly to the J3 Connector on your MicroZed Board if you are using it 'standalone' and powered from the USB connector. If you have the MicroZed plugged into a Carrier Card you will need to connect the programming cable to the Carrier Card JTAG connector.

     

    Then I would suggest you take a look at the MicroZed tutorials available on the MicroZed Reference Designs page:

     

    http://zedboard.org/support/design/1519/10

     

    There are also solution files for the tutorials as well as instructions for programming the QSPI Flash on the same page.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • raymadigan
    0 raymadigan over 10 years ago in reply to e14 Contributor

    I have the HS2 RevA cable. 

    Thank you for the reference.  I had actually downloaded one of the pages before.  I did get further because:

    1. Set the Boot Mode jumpers to Cascaded JTAG Mode.

    Which I didn't know before.  Now I get the message that it can't find the fpga.  I am sure the cable is setup correctly, but I can't find how to set the Xilinx/Digilent cable switch settings.   In previous SDK there was a menu item to accomplish this which is not available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • raymadigan
    0 raymadigan over 10 years ago in reply to e14 Contributor

    I have the HS2 RevA cable. 

    Thank you for the reference.  I had actually downloaded one of the pages before.  I did get further because:

    1. Set the Boot Mode jumpers to Cascaded JTAG Mode.

    Which I didn't know before.  Now I get the message that it can't find the fpga.  I am sure the cable is setup correctly, but I can't find how to set the Xilinx/Digilent cable switch settings.   In previous SDK there was a menu item to accomplish this which is not available.